Publications
  • Learn
  • More
Publications
Blog New turbine design works in urban areas
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 17 May 2011 6:45 PM Date Created
  • Views 1617 views
  • Likes 1 like
  • Comments 6 comments
  • turbine
  • alternative_energy
  • wind
  • dit
  • eavesdropper:dit
  • industry
  • energy
  • innovation
Related
Recommended

New turbine design works in urban areas

Eavesdropper
Eavesdropper
17 May 2011
imageimage
 
There are major issues with using wind turbines in urban areas. Ice whipping from the blades and other mechanical disasters face turbine use on a regular basis. However, safer and smaller turbine arrays have been shown to be a major benefit. The goal is to get a larger turbine safe enough for use in cities. Katru Eco-Energy may have found the perfect balance with their IMPLUX vertical turbine. This turbine is omni-directional, somewhat enclosed, and can use up to 87% of the wind that moves into its housing. The side walls of the turbine are shaped in such a way to force the air entering to move upwards through the actual turbine blades. And birds can not be pulled into the turbine and killed, do not worry. The slots are too small for them to pass through. Which does not mean that will not get stuck in there. The first IMPLUX turbine will be approximately 4m in diameter and produce 2 KW. And future models, Katru boasts, will output 4 - 10 KW.
 
The IMPLUX was first demonstrated at the Engineering Excellence Awards, Sydney-Australia, back in 2007. The United States patent was awarded in 2008. And the first production model will be available in 2012. A long development indeed.
 
Eavesdropper
 
Pictures and  Video via Katru
  • Sign in to reply

Top Comments

  • DAB
    DAB over 15 years ago in reply to Eavesdropper +1
    Actually, the wind IS solar powered. The heating and cooling cycles as the earth turns provides the energy for up and down drafts within the atmosphere. So given all of the radiative heating going on,…
Parents
  • DAB
    DAB over 15 years ago

    It would be interesting to see how this approach compares to the helix based wind turbine developed in Chicago.  It was a much simpler design, bird safe and could run either verticle or horizontal with full over spin compensation.

     

    Thanks,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 15 years ago

    It would be interesting to see how this approach compares to the helix based wind turbine developed in Chicago.  It was a much simpler design, bird safe and could run either verticle or horizontal with full over spin compensation.

     

    Thanks,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Eavesdropper
    Eavesdropper over 15 years ago in reply to DAB

    This one, Dab? I took a picture of it at the Chicago Planetarium.

    image

    I too would like to know the efficiency of this turbine vs others. I will look into it.

     

    E