Publications
  • Learn
  • More
Publications
Blog Permanent magnet motor, how it works and when to see it in use
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 1 Nov 2011 6:37 PM Date Created
  • Views 1050 views
  • Likes 1 like
  • Comments 1 comment
  • alternative_energy
  • transportation
  • industry
  • magnet
  • permanent
  • innovation
Related
Recommended

Permanent magnet motor, how it works and when to see it in use

Eavesdropper
Eavesdropper
1 Nov 2011

image


General Motors (GM) teaches us about, while promoting, their new permanent magnet (PM) electric motor. Forcing out 114 hp (85 kE) of torque, the new motor is set to be central to the Chevrolet Spark electric vehicle coming out in 2013. Of course, the full 114 hp will not be completely sustained during all operations, only about 75 hp can be maintained. However, peak power is available when the motor starts up, delivering instant torque.
 
A permanent magnet motor does not have a field winding on the stator. The permanent magnets provide the magnetic field for the rotor field to interact. In this case, there are windings on the permanent magnet ring, which are used to improve commutation under load. Large PM motors are not very common due to cost and difficulty with assembly. It has been difficult to find a material able to retain the high-strength field needed. Only with recent developments with neodymium magnets has GM, or any company, been able to use PM motors for large applications.

GM never mentioned the issues that might rise from the use of PM motors. Over saturation of the PM core can lead to over voltages or other control reliability issues. Occasionally, air gaps in the material left over after manufacturing may have to be repaired. Assembling of PM motors are also fraught with problems, electrocution being the biggest. High performance permanent magnets have inherent structural and thermal issues. As more work is done with PM materials, I am sure the issues can be subdued.

 
This may usher in a the wave of electric vehicles the world needs.
 
Eavesdropper
  • Sign in to reply
  • DAB
    DAB over 14 years ago

    I have to admit, GM did a very good job of explaining how their new electric motor design works and why it is useful.

     

    My only complaint against electric vehicles has been that they use electricity inefficiently generated by a coal fired power plant.

     

    After seeing their design, It would be very interesting to see the accelleration the new motors can put out on a full charge.

     

    DAB