Publications
  • Learn
  • More
Publications
Blog Petri dish scanning using cell phone and LEGOs
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 12 Oct 2011 7:24 PM Date Created
  • Views 819 views
  • Likes 1 like
  • Comments 1 comment
  • research
  • test
  • dit
  • eavesdropper:dit
  • medtronic
  • on_campus
  • measurement
  • university
  • medical
  • innovation
Related
Recommended

Petri dish scanning using cell phone and LEGOs

Eavesdropper
Eavesdropper
12 Oct 2011
image
ePetri patform of cell phone and LEGOs (left), imaging sensor (right)
 
 
The California Institute of Technology, CalTech, has built a new way to culture cells using LEGOs, a smartphone, and some high tech imaging devices that will change petri dish usage forever. Guoan Zheng, grad student and author of the study, explained, "Our ePetri dish is a compact, small, lens-free microscopy imaging platform. We can directly track the cell culture or bacteria culture within the incubator. The data from the ePetri dish automatically transfers to a computer outside the incubator by a cable connection. Therefore, this technology can significantly streamline and improve cell culture experiments by cutting down on human labor and contamination risks."
 
A few of the features will help it take dominance in the medical field. The complete system, built around legos, is sealed in an incubator, which keeps contamination due to handling to an absolute minimum. The imaging sensor can  take rapid wide-angle  pictures of the Petri dish, which are immediately transferred to a computer and pieced together into a larger high-resolution image. The on-chip imaging  is based on subpixel perspective sweeping microscopy (SPSM).
 
Senior author of the study, Professor Changhuei Yang, said, "Until now, imaging of confluent cell cultures has been a highly labor-intensive process in which the traditional microscope has to serve as an expensive and suboptimal workhorse. What this technology allows us to do is create a system in which you can do wide field-of-view microscopy imaging of confluent cell samples. It capitalizes on the use of readily available image-sensor technology, which is found in all cell-phone cameras."
 
According to the study, the cell phone is only used for its LED screen as a scanning light source. Although some phones, in this case an Android phone, can be inexpensive, it seems like a waste to use the whole phone for just back lighting. I am sure there are cheaper alternatives.
 
The team believes that their scanner will open up new possibilities for portable diagnostic lab-on-a-chip tools. Other areas they will be pushing the tech are in drug screening, detection of toxic compounds, and stem cell research. 
 
Let's hope the final design is not laying on LEGOs. I would not assume there is high precision between blocks.
 
Eavesdropper
  • Sign in to reply
  • DAB
    DAB over 14 years ago

    Hi E,

     

    An interesting application.  I agree, if they used one of the small microscope cameras, they could use it to capture the data inside the sterile environement and bring our the video/image to a bigger screen.  I like the idea of using the Legos.  They would help you set up different types of  dish sizes for the scanning.  It would be very easy for them to set up an X-Y dish extractor and use the legos to build a matrix of the cultures being grown.  The dish extractor could cycle through the matrix, pull out each dish, take it over to the camera, take the picture, return the dish and go to the next.

     

    A simple Arduino or MSP430 could handle software.  You already have many designs for and X-Y motor driven device.  The rest is a simple robot sampling task.

     

    Just a thought,

     

    DAB