Publications
  • Learn
  • More
Publications
Blog Rectenna to scavenge energy from microwave-ovens (up to 100W)
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 12 Dec 2011 8:56 PM Date Created
  • Views 1095 views
  • Likes 1 like
  • Comments 1 comment
  • alternative_energy
  • rfid
  • cabeatwell
  • transformer
  • rectenna
  • energy
  • microwave
Related
Recommended

Rectenna to scavenge energy from microwave-ovens (up to 100W)

Catwell
Catwell
12 Dec 2011
image
Rectenna from Dengyo (via Dengyo)
 
A rectenna is a type of antenna that converts microwave energy into DC. Usually arranged in a "multi element phased array with a mesh pattern reflector element," a rectenna ends up being directional. RFID is a common use of rectenna tech. (Side note: a Schottky diode is placed across dipole antenna elements, rectifying the AC current induced by microwaves.)
 
Japanese company Nihon Dengyo Kosaku Co Ltd (Dengyo) has created a rectennas for the 2.4GHz band of microwave energy. Although the rectenna could  pick up 6mW from Tokyo Tower at 4 km away, the device is being pushed as a great way to recover lost energy in microwave heating products, such as a microwave-oven. The rectenna re-collects energy not used to heat the food.
 
The team claims that foods with a low-water  content have a high regeneration efficiency, meaning they recover more energy. The microwave oven rectenna formula breaks down as follows (From Dengyo):
ηt = ηm x (1 - ηh) x (1 - LC) x ηr x ηC
ηm is the efficiency of converting alternating-current power into microwaves with a microwave oven
ηh (heating efficiency) is the ratio of the energy used for heating food or materials to the energy of the generated microwaves
LC is the loss of the transmission circuit
ηr is the efficiency of the rectifier
ηC is the efficiency of the boost circuit or superposed circuit
Case 1: ηm = 70%, LC = 10%, ηr = 80%, ηC = 90% ηh = 50% yields ηt = 22.7%
Case 2: ηm = 70%, LC = 10%, ηr = 80%, ηC = 90% ηh = 10% yields ηt = 40.9%
 
Up to 100W can be reclaimed from the 103 x 93 x 17mm rectenna. Time to extend our planet's resources while cooking the usually dry dinners we end up stomaching.
 
Cabe
http://twitter.com/Cabe_e14
  • Sign in to reply
  • DAB
    DAB over 14 years ago

    Hi Cabe,

     

    It would be very interesting to see what affect these devices have on the microwave transmitter.  I am not sure if a passive device like this could cause RF scattering or create far field energy distribution affects.  There are lots of interesting things that happen when you change a microwaveform structure, especially in free space.

     

    Thanks for the post.

    DAB