Publications
  • Learn
  • More
Publications
Blog Refrigerator-Sized Anechoic Chamber
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: gervasi
  • Date Created: 12 Oct 2011 6:52 PM Date Created
  • Views 1026 views
  • Likes 1 like
  • Comments 2 comments
  • mimo
  • test
  • cgervasi:dit
  • measurement
  • rf
Related
Recommended

Refrigerator-Sized Anechoic Chamber

gervasi
gervasi
12 Oct 2011

OctoScope’s new refrigerator-sized anechoic chamber, called the octoBox, reminds me of past projects involving RF and EMI testing.  When I was at Jabil Circuit, they had a nice 100 sq ft walk-in chamber. The DUT and antennas could be placed in the chamber with the “master” and the test equipment outside.  In practice, we often moved the test equipment into the chamber so we could make changes to the DUT and get immediate feedback by looking over at the test equipment.  The chamber had white lights illuminating the equipment and non-reflective black tiles on all sides of the room.  Even the most cheerful person would experience some sense of sensory deprivation after spending most of the day working in the room.
image


I have never worked with a small chamber like octoBox, but I imagine the time spent opening and closing the doors would be less than the time gained by not having to leave the room to look at the test equipment.  OctoBox is divided into two chambers: one for the master and a larger one for the DUT and antennas.  The isolation between the two chambers is 80dB at 6GHz, 90dB and 2.4GHz, and around 100dB at VHF and UHF frequencies.   Isolation between the chambers and the outside world is around 80dB.  The walls reflect -20dB of incident waves.


One application of a small chamber is testing MIMO devices with various channel emulations.  In MIMO, antennas are an important part of the channel model, so you cannot simply put the DUT in an RF shielded enclosure and connect the channel emulator to the DUT through coax and attenuators.  image


Wireless devices increasingly have integrated antennas.  Lab testing with the devices’ actual antennas, even when the radios are not MIMO, is better than soldering coax to the antenna connections.  For functional test in production, an over-the-air test is the only option.  Automated test equipment can be configured to test multiple devices at once in the chamber. 


Even without expensive equipment like a channel emulator, it would be nice to have a large anechoic box to pre-test products to get an idea of whether they will pass EMI emissions testings and to be able to test transceivers with real antennas in a repeatable way in the lab.

  • Sign in to reply
  • Former Member
    Former Member over 14 years ago in reply to DAB

    DAB, great idea to add temperature cycling.  octoBox is easily customzable and we appreciate your thoughts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 14 years ago

    It would be a good place to do some life cycle signal degridation testing.  Did they say they could control the temperature, humidity, pressure, etc?  I could see those issues needing to be addressed for most devices.

     

    I can also see this unit being used to test many of the new miniature robots and signal snoopers.  You could run a good baseline on each device to establish a baseline.  However, I agree with you about the access.  It would be very useful to have a sliding door to place and remove the devices quickly for basic testing.

     

    From the specifications, it looks like they are aiming at the wireless market for manufacturers to verify FCC compliance and to look for crossband interferrence issues.

     

    Could be an interesting tool though.

     

    DAB

     

    By the way, have you ever heard of the BAAF?  If so, send me a private email and we can discuss its interesting issues.

    • Cancel
    • Vote Up 0 Vote Down