Publications
  • Learn
  • More
Publications
Blog Researchers design cylinder with cloaking capabilities
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 27 Mar 2012 5:32 PM Date Created
  • Views 612 views
  • Likes 1 like
  • Comments 1 comment
  • research
  • test
  • hmi
  • on_campus
  • cloaking
  • cabeatwell
  • prototyping
  • measurement
  • wireless
  • university
  • energy
  • scan
  • mri
  • sensor
  • innovation
Related
Recommended

Researchers design cylinder with cloaking capabilities

Catwell
Catwell
27 Mar 2012

image

Concept (via Universitat Autonoma de Barcelona)

 

Slowly but surely, the cloaking devices seen on almost every sci-fi show in existence are becoming a reality. Sure we can’t actually hide a Klingon Warbird (we haven’t figured out how to build one yet), but we can do the next best thing, cloaking objects from magnetic fields. A collaboration with researchers from the Universitat Autonoma de Barcelona (Spain) and the Institute of Electrical Engineering (Slovakia) have designed a special cylinder that is able to hide objects from magnetic fields.

 

The research team was able to build the device using a super-conductor material encased in iron, nickel and chrome (chrome for style?). There are two main layers. One is a superconductor that reflects magnetic fields, while the other ferromagnetic layer attracts the same fields. Anything placed inside a cylinder of the composite materials will be undetectable. Think of it as being able to bend a magnetic field around an object. Theoretically you could pass through a metal detector at an airport with anything that could fit inside the cloaking tube undetected. That is until security notices the liquid nitrogen vapor (used for the superconductor) coming off the metallic cylinder. All kidding aside, the technology could be adapted for use in the medical field to shield pacemakers or other implants from magnetic resonance tests, as well as a host of other applications.

 

Cabe

http://twitter.com/Cabe_e14

 

Engineering On Friday shows the military application for this tech.

  • Sign in to reply
  • DAB
    DAB over 14 years ago

    Hi Cabe,

     

    There are several techniques to make objects undetectable to certain detecting devices.

    A true "Cloak" would need the ability to remain undetectable to a wide range of detecting devices.

    I am not sure that I can see a benefit to this research as I do not understand the area in which making something undetectable is useful to the general populace.

     

    Just my opinion.

    DAB