Publications
  • Learn
  • More
Publications
Blog Researchers develop Wi-Fi-based passive radar that can see through walls
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 14 Aug 2012 6:50 PM Date Created
  • Views 643 views
  • Likes 1 like
  • Comments 1 comment
  • research
  • defense
  • test
  • military
  • industry
  • hmi
  • law_enforcement
  • on_campus
  • cabeatwell
  • prototyping
  • measurement
  • sensor
  • innovation
  • communication
Related
Recommended

Researchers develop Wi-Fi-based passive radar that can see through walls

Catwell
Catwell
14 Aug 2012

image

Concept art (via Kevin Hard & Teknisk Ukeblad)

 

Those looking to commit crimes by hiding out where no one can see them, better think again. WiFi signals bathe other everything, including criminal activity. Law enforcement may employ a high-tech toy in the form of a Passive Bistatic WiFi Radar that can see through walls. The bad guys can't hide. (This is similar to the "Doppler" radar Batman used in the film "The Dark Knight.")

 

image

Signal process, how it can see through walls (via Locating a moving target in a high clutter environment)

 

Developed by researchers Karl Woodbridge and Kevin Chetty (from University College London), the design works similar to Doppler radar, which tracks the velocity and location of an object using radio signals (the frequency changes when it hits a target). However, their detection system uses WiFi-based signals to track an individual’s location, speed, and direction through high-clutter indoor environments, as opposed to weather or aircraft. The pair’s system was designed using a 2.4-GHz passive multi-static receiver (the size of a suitcase) that is equipped with two antennae with one used to monitor base WiFi signals in a given hotspot and the other to monitor reflected WiFi signals that have changed frequencies. The receiver takes the WiFi data and sends it to a computer where it analyzes the signal discrepancies and pinpoints the targets location. For example; the device can take a base-line reading (usually 2.4 or 5GHz) from your router in your residence. When you move closer or further from the router its signal changes to either a higher frequency or lower depending on your distance. By comparing the base-line to the altered signal, the system can pin-point your location (within a few feet) in real-time.

 

The researcher’s state that with a little more development they can refine their system using what’s known as a ‘Clean algorithm’ (de-convolutes an image in radio astronomy based off of a series of point sources). This would clean up any static interference and make their system sensitive enough to detect a person’s rib-cage movement while breathing!

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • gervasi
    gervasi over 13 years ago

    This sounds fantastical, but it's totally viable.  802.11(n) uses MIMO to send multiple streams at the same time on the same frequency using the multipath reflections in the channel.  In an indoor environment, there is also a reasonably rich delay spread, which the paper calls a "high-clutter environment".  So this is very possible.  This works using only signals coming from the property; it doesn't require signals from the spies, so it will be an interesting legal question as to whether this requires a warrant. 

     

    This came up in the Supreme Court case involving GPS tracking.  The justices said it requires a warrant for law enforcement go on someone's property, but one justice looked ahead and said soon this tracking will be possible w/o going on someone's property, and we'll have to deal with that at that time.