Publications
  • Learn
  • More
Publications
Blog Scientists create plastic that mimics human skin, bleeds and self-repairs
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 29 Mar 2012 5:49 PM Date Created
  • Views 759 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • test
  • industry
  • material_engineering
  • robotics
  • robot
  • on_campus
  • Design
  • plastic
  • cabeatwell
  • prototyping
  • university
  • technology_for_the_disabled
  • material_science
  • sensor
  • innovation
Related
Recommended

Scientists create plastic that mimics human skin, bleeds and self-repairs

Catwell
Catwell
29 Mar 2012

image

Cencept of how the plastic repairs (via American Chemical Society)

 

The day may come when our robot subordinates will be able to bleed and bruise when we suppress their uprising, thanks to a new form of polymer that has self-healing capabilities. At this year’s ACS (American Chemical Society) Professor Mark W. Urban (School of Polymers and High Performance Materials at USM) unveiled a new type of plastic his research group has designed that mimics human skin in that it can discolor and even bleed, which is needed for the healing process, when damaged. The polymer works similar to skin in that when exposed to UV light, temperature or pH fluctuations it changes to shades of red when damaged and bleeds when cut or scratched.

 

The secret to this is that the team’s water-based copolymers is infused with nano-links, dubbed ‘bridges’, that travers the chemical make-up of the plastic. Once damaged these tiny links distort and change shape resulting in a red color. Once these deformities are exposed to light or temperature changes the nano-links return to their original state which gives the plastic its self-healing properties. The applications for which this new polymer can be applied to are virtually endless. Think of it being incorporated into cars (self-healing fenders?), planes (stress-point identifiers), body armor (heals after round impact), medical applications (burn victims, artificial limbs), and the list goes on and on. What might you apply it too? Let’s hear some feedback.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • DAB
    DAB over 13 years ago

    Hi Cabe,

     

    Did the article indicate if the new "skin" could be used for severe burn cases?

    This development could be a real boost for people who need synthetic skin while they heal from extreme burns or injuries.  It could help a lot of people.

     

    Good post,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 13 years ago in reply to DAB

    DAB,

     

    They call it skin, but that is a bit of a misnomer. It is only meant for inorganic surfaces. There are plenty of medical technology out there that would be a better use for burn or trauma victims.

     

    The above skin may never be used for medical.

     

    Cabe

    http://twitter.com/Cabe_e14

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Catwell
    Catwell over 13 years ago in reply to DAB

    DAB,

     

    They call it skin, but that is a bit of a misnomer. It is only meant for inorganic surfaces. There are plenty of medical technology out there that would be a better use for burn or trauma victims.

     

    The above skin may never be used for medical.

     

    Cabe

    http://twitter.com/Cabe_e14