Publications
  • Learn
  • More
Publications
Blog Scientists create polymer circuits printed with the help of laser ablation
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 26 Nov 2012 7:53 PM Date Created
  • Views 455 views
  • Likes 0 likes
  • Comments 0 comments
  • research
  • industry
  • hmi
  • manufacturing
  • circuit
  • on_campus
  • circuit_printing
  • embedded
  • cabeatwell
  • prototyping
  • measurement
  • printing
  • university
  • innovation
  • communication
Related
Recommended

Scientists create polymer circuits printed with the help of laser ablation

Catwell
Catwell
26 Nov 2012

image

Printing concept (via Laser Induced Forward Transfer of conducting polymers)

 

Printed polymer circuits have been adapted for use in a wide range of electronics, including smartphones, keyboards and thin solar films. While they are incredibly robust and provide many advantages (cheap to produce, flexibility and lightweight), the conductive polymer (plastic) has its drawbacks, most notably in the manufacturing techniques used to create them. Leading research may have a solution.

 

Typically, most conductive polymers are created using ‘oxidative coupling of monocyclic precursors’ (or a compound creating another compound through a chemical reaction comprised of some pretty nasty hydrocarbons such as benzene). This process entails using a liquid polymer with a solvent that’s then can either be sprayed or inkjet coated (a form of printing) onto a substrate. However, this process has the tendency to dissolve the layer below (if that layer is also a polymer) or has the capacity of coalescing into a ring (known as the ‘coffee ring affect’) with the polymer concentrating at the outer edge of a droplet. Scientists from the National Technical University of Athens (Greece) have found a novel way around these problems by incorporating laser printing in their manufacturing process.

 

Led by Maria Kandyla, the team used laser ablation (or vaporization of material) to deposit a conductive polymer onto the substrate rather than using the solvent method to make a circuit. To make the circuit, the team first deposited a layer of conducting polymer on a substrate of glass (called the ‘donor substrate’), which is done by the more traditional method of spin-coating - allowed to cure (just like it sounds; a dab of liquid polymer material is placed in the center of the substrate and then rotated at high speed). The team then placed the ‘receiving’ substrate next to the face of the donor, separated by a few micrometers, and then a laser is fired through the glass substrate which dissolves or detaches a small amount of the conductive polymer onto the receiving substrate. The circuit is created by moving the two substrates during the laser-firing process to deposit 2D patterns (in any shape), which makes the circuit. Since the transfer process is done with solid polymers, the problems associated by using solvents is avoided. So far the team has tested their method successfully using P3HT:PCBM, which is commonly found in thin-film photovoltaic cells, as well as using polyaniline to print up biological sensor circuits. Perhaps more than organic LEDs will be made with the process in the near future.

 

Cabe

http://twitter.com/Cabe_e14