Publications
  • Learn
  • More
Publications
Blog Sharing the RF Spectrum
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: gervasi
  • Date Created: 28 Jul 2012 8:24 PM Date Created
  • Views 681 views
  • Likes 1 like
  • Comments 2 comments
  • spectrum
  • policy
Related
Recommended

Sharing the RF Spectrum

gervasi
gervasi
28 Jul 2012

In the 80s I frequently heard claims about frequency space being scarce.  Mobile phone providers were growing and they wanted more spectrum.  They were having to decrease the size of their cells so that they could reuse the spectrum they had.  The more spectrum they had, the less reuse was needed.  Other services, such as public safety and even amateur radio operators, said their bands were packed.  image

 

I recall repeating this claim to a friend around 1990.  He said, “I keep reading that, but I don’t see it when I tune down any band above 30MHz.  It’s mostly unused.”  It struck me because I had observed the same thing but never thought about it as evidence against spectral scarcity.  A year later when my family was on vacation, they took me to Sears tower.  When we arrived at the observation deck, I tuned along the 460MHz public safety band.  Every 25kHz, and in some cases 12.5kHz, I heard a station.  When that station stopped transmitting, there were weaker stations behind it.  I surveyed every band my handheld could receive for the rest of the time we were there, without taking notice of the exhibits and without it ever occurring to me what a nerd I was. 

 

It etched in my mind that at a high elevation in an dense urban area, the spectrum was indeed crowded.  Trunking systems, in which say 50 users whose usage duty cycle is well under 20% can share 10 frequencies, were being introduced at the time.  A decade later Wi-Fi became common.  The 2.4GHz band is about 80MHz wide, big enough to fit three non-overlapping 22MHz channels.  Three channels sounds like way too few, but 802.11’s channel access scheme does an excellent job of sharing a channel among many uncoordinated users.  Several office networks and a coffee shop can all use the same channel without users typically noticing a degradation in throughput.  The collision avoidance scheme allows them to share the bandwidth fairly.

 

image

When I first observed this I thought it was a clear example of a libertarian approach providing vastly better results than a government approach.  Wi-Fi equipment typically has a country setting so that the device can obey the laws of the country where it’s deployed.  I used to joke there should be a “Somali country code” that would let the device do whatever it wanted.  Somalia at the time had no functioning government yet had some of the best mobile phone service in Africa, partly because it didn’t have government corruption impeding deployment of wireless technology.  My first post for element14 argued for that self-interested devices would have an incentive to share the channel nicely in exchange for reciprocity from other devices. 

 

I recently watched an IEEE tutorial on dynamic spectrum markets, though, and learned the pure libertarian model is simplistic.  The presentation breaks down channel access into three types: exclusive use (e.g. TV and radio stations), commons (e.g. Wi-Fi), or hierarchical (e.g. DFS Wi-Fi channels that devices must abandon if they detect another service using the channel).  The common model only works well if spectrum isn’t too scarce.  For short range communication at >3GHz, spectrum is not scarce, so this model works well.  The model does not work as well for services that cover a larger area. 

 

The IEEE presentation argues for the creation of some system that allows users to rent the use of a frequency range for a short time in a very limited area, such as for a few minutes within range of a single access point. 

 

For the next few decades, I believe bandwidth for short-range use will remain plentiful.  The 5-6GHz (a) band of Wi-Fi is still underutilized is most places.  Higher frequency bands can be made available if it becomes crowded.  Techniques like MIMO and CDMA can increase the amount of data sharing the channel. 

 

In rural regions, there will be plenty of bandwidth even for services covering a broad area.  Urban regions, will follow the pattern of renting commercial or residential space in a dense urban area with prices shockingly high to people from less densely-populated.  As with many issues, rural people will want a more laissez-faire approach and urbanites will want a strong Leviathan to maintain a framework for people to live together in close proximity in peace. 

 

When making spectrum use policy, we should avoid a one-size-fits-all approach for entire countries.  We need a way to allow a device to hog all the spectrum in a rural field but negotiate a rental price when the same device is located in a place like the Sears Tower. 

  • Sign in to reply
  • gervasi
    gervasi over 13 years ago in reply to DAB

    It amazes me how in most locations there is no congestion.  Even in downtown Madison, 802.11's channel access scheme is good enough that you can have 20 networks visible and still have 10 people surfing the web or using apps in a coffee shot, all on the same frequency without noticing too much congrestion.  Most people aren't even using the 5GHz 802.11 channels yet.  In a channel with a reasonable delay spread, you can double the capacity just by going to 2-stream MIMO with 802.11(n). 

     

    I suspect there is bona fide congestion on WiFi (ISM bands) and other bands in places like NYC or Amsterdam.  They'll need a solution to share/rent that common resource efficiently.  It's much less of a problem in Madison.  In the north woods, it's not an issue at all.  It would be nice for devices to recognize they're in a low-population-density area and be freed to use more power and frequency space.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 13 years ago

    I suspect you are right.

    The issue of fair allocatioin varies from person to person and from business to business.

    In the end, we probably need to put a user tax on bandwidth use.  It is only fair to have those who use the most spectrum pay the most for its use.

    You can see this example being played out with ATT and Verizon as they have a few Mega Users and many more normal users.  They eventually had to shut down the unlimited data plans except for those people who were willing to pay a lot for the service.

    The sad thing was the content they were paying to see.  I personnaly found it unbelievable as to what things people were willing to pay big bucks to see.

     

    Oh well, I digress.

     

    I wonder how long we go before some more advanced species arrives and tells us to stop clogging their spectrum with useless noise?

     

    In the meantime you need to think about what you want to do with the RF spectrum and think about what makes sense.

    Until then, chaos will reign and the noise across all spectra will increase.

     

    Just my opinion,

    DAB