Publications
  • Learn
  • More
Publications
Blog Silicon as the New PCB?
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: DaveYoung
  • Date Created: 7 Dec 2012 2:02 PM Date Created
  • Views 826 views
  • Likes 2 likes
  • Comments 2 comments
  • test
  • soc
  • keithley
  • analog_engineering
  • measurement
  • dyoung
  • national_instruments
  • analog_devices
Related
Recommended

Silicon as the New PCB?

DaveYoung
DaveYoung
7 Dec 2012

image“Chips will continue to swallow board functions” image

“Size, complexity, development time, and cost requirements are making individual components an expensive luxury”

 

As chip manufacturers continue to get better and better with integrating functionality on System on a Chip (SOC) devices, engineers are saying things like those listed above.  It is true that the industry of making Integrated Circuits (ICs) is becoming more and more advanced every day.  Some of the smartest people are behind the blazing rate of technology growth in that area, and given the ever-increasing market for portable devices it is no wonder IC manufacturers are investing in that direction.

 

A friend recently pointed me in the direction of 'Analog Front End' (AFE) chips that have become almost an entire stand alone circuit capable of interfacing directly with the physical world.  With my love of analog electronics and experience developing precision measurement equipment, I was excited to look closely at the new technology advances.

 

The holy grail for chip manufacturers is to allow an engineer to design in the AFE IC, adding only user inputs/outputs and a microcontroller/FPGA, to complete the hardware development.  It's certainly a tantalizing thought given the risk, time, and expense involved when designing analog systems from discrete components or even with analog ICs like op amps.  But are we there yet?

 

To answer how close they are, I've read the specs of the AFE chips and compared them with a couple complete products that can be bought today.  The AFE is Analog Devices' AD 5520, a Per Pin Parametric Measurement Unit/Source Measure Unit.  This is very similar to Keithley's entry-level 2401 SourceMeter Instrument and the module-based National Instruments PXIe-4140 Source Measure module.

 

The datasheets for all of these devices are pages long, so I'll boil them down to the specs which most users will find important.  Please consider these figures to be approximate as some massaging was required to give comparable figures.

 

SpecificationAD5520KI 2401NI 4140
General Capabilities


Max Voltage Output+/- 11V+/- 20V+/- 10V
Max Current Output+/- 4mA+/- 1A+/- 100mA
Max Power Output44mW20W1W




Voltage Source


Gain Error1%, max10.17%, max1+/- 0.125% max1
Offset Error+/- 1mV+/- 0.6mV+/- 5mV
Current Source


Gain Error1%, max10.29%, max10.2%, max1
Offset Error<not spec'd>+/- 0.6nA+/- 5nA




Voltage Measurement


Gain Error+/- 0.03%+/- 0.012%+/- 0.1%
Gain Error Tempco2 ppm/°C18 ppm/°C5 ppm/°C
Input Offset Error+/- 5mV+/- 0.3mV+/- 5mV
Input Offset Tempco+/- 15uV/°C+/- 45uV/°C+/- 1uV/°C
CMRR (Noise)73dB100dB<not spec'd>
Current Measurement


Gain Error0.10%0.03%0.10%
Gain Error Tempco30 ppm/°C40 ppm/°C20 ppm/°C
Input Bias Current+/- 1nA+/- 60nA+/- 500nA
Input Bias Current Tempco+/- 50 pA/°C+/- 9nA/°C+/- 1nA/°C
CMRR (Noise)95dB100dB<not spec'd>




Retail Price (in single quantities)$33.46$3,120.00$4,699.00

Footnotes:

1. 'Max' designates spec over 0-70°C temperature range, compared to the stndard 25*C fixed.

 

Clearly these three are totally different products far from being interchangeable, especially since the IC will require additional components adding errors and cost while the completed units are ready to go.  And after reading through the AD5520 spec sheet, there is still a large amount of analog development that is required to properly use the chip.  So no, analog design isn't dead.  But it's impossible to ignore the incredible progress and integration on the chip level, and easy to imagine the future possibilities.

 

Has anyone used one of these AFE-type chips?  Are they as easy and as accurate as the documentation suggests?  Are there any unexpected surprises that are found in development?  Let us know in the comments!

  • Sign in to reply
Parents
  • DAB
    DAB over 13 years ago

    Hi Dave,

     

    I must point out that Analog design will never die!  Digital is a subset of Analog.

     

    As for putting more functions on silicon, a lot of us designers have pushed for that development for decades.  One reason was the time it took to layout the boards, sending them off to be made, correcting manufacturing or design errors and then finally getting down to debugging the device we designed.

     

    Granted, the new CAD tools have made the board development process easier, but for a long time it was just too cost prohibitive to do.

     

    I think a lot of designers would like to design a circuit and have a silicon chip pop out of a machine ready to hook up and test.  I see this capability evolving from the technology, but until then, we must still work with SOC, IC's and all of the other bits to make a working product.

     

    That said, I am also eager to hear from others on their experience with the SOC chips you mentioned.  It would be interesting to see someone do a comparison of the chips to see if they are indeed solving the same problem or if they just have similar specs.

     

    Good post.

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 13 years ago

    Hi Dave,

     

    I must point out that Analog design will never die!  Digital is a subset of Analog.

     

    As for putting more functions on silicon, a lot of us designers have pushed for that development for decades.  One reason was the time it took to layout the boards, sending them off to be made, correcting manufacturing or design errors and then finally getting down to debugging the device we designed.

     

    Granted, the new CAD tools have made the board development process easier, but for a long time it was just too cost prohibitive to do.

     

    I think a lot of designers would like to design a circuit and have a silicon chip pop out of a machine ready to hook up and test.  I see this capability evolving from the technology, but until then, we must still work with SOC, IC's and all of the other bits to make a working product.

     

    That said, I am also eager to hear from others on their experience with the SOC chips you mentioned.  It would be interesting to see someone do a comparison of the chips to see if they are indeed solving the same problem or if they just have similar specs.

     

    Good post.

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • DaveYoung
    DaveYoung over 13 years ago in reply to DAB

    DAB-

    I should have mentioned your excellent point in the article: We will have analog electronics as long as we live in the analog world!  Still, I think their goal is to enable an engineer to pipe a user's signal directly into a pin on a chip.  Analog engineering is still a big part, but the focus is far different than setting up current mirrors with matched JFETs. 

     

    As always, it's an exciting time!