Publications
  • Learn
  • More
Publications
Blog Single molecule performs 13 logic operations
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 23 May 2011 9:11 PM Date Created
  • Views 674 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • test
  • dit
  • eavesdropper:dit
  • on_campus
  • single_molecule
  • molecule
  • measurement
  • university
  • innovation
Related
Recommended

Single molecule performs 13 logic operations

Eavesdropper
Eavesdropper
23 May 2011
image
FG-DTE Molecule and functions
 
A photonic controlled molecule that can perform 13 logic functions that are reconfigurable via changing the input/output wavelengths of light. The chromophores, the part of the molecule responsible for its color, absorbs certain wavelengths of light. States of the molecule can change depending on the light entered, this created photoswitchable, bitstable chromophores, called photochromes. Researchers from Chalmers University of Technology in Göteborg, University of Huelva, and Arizona State University have created a light-sensetive molecule based on these properties made of one dithienylethene (DTE) and two fulgmides (FG). The combination FG-DTE, for example, can change states with inputs of 302 nm  and 397 nm, performing addition and subtraction. All molecules can be reset with green-light in the 460-590 nm range. Researcher Joakim Andréasson, from Chalmers, said  All of these 13 logic operations share the same initial state, that is, the molecule is always ‘reset’ to one and the same state by the use of green light, irrespective of which logic function is to be performed. This is another unique feature of our molecule.”
 
The FG-DTE can also work non-arithmetic functions, digital multiplexor, demultiplexor, and most importantly sequential logic. However, stability over repeated state changes is not consistent. This and string concatenation are the researcher's priority in the coming months. 
 
Eavesdropper
 
pic via Joakim Andréasson
  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    I will bet you thought I was crazy to suggest using photons to build logic circuits?

     

    The potential for this compact form of circuitry could really make a significant impact on future devices.  I can't wait to see what they do next.  Thirty years ago, IBM expected to reach memory devices with Terabits per CM3.

     

    Thanks,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Eavesdropper
    Eavesdropper over 14 years ago in reply to DAB

    Not at all.

    Though not as immediate, I really like the pure light based transistor concept. It does work too.

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Eavesdropper
    Eavesdropper over 14 years ago in reply to DAB

    Not at all.

    Though not as immediate, I really like the pure light based transistor concept. It does work too.

     

    E