Publications
  • Learn
  • More
Publications
Blog So sweet. Boeing future planes to go green with SUGAR.
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 28 Mar 2012 6:18 PM Date Created
  • Views 1246 views
  • Likes 1 like
  • Comments 1 comment
  • research
  • alternative_energy
  • defense
  • test
  • transportation
  • military
  • green
  • aircraft
  • industry
  • hmi
  • nasa
  • Design
  • cabeatwell
  • prototyping
  • measurement
  • energy
  • sensor
  • innovation
Related
Recommended

So sweet. Boeing future planes to go green with SUGAR.

Catwell
Catwell
28 Mar 2012

image

(Left) SUGAR high/freeze (Right) supersonic Boeing concept (via Boeing)

 

"Green" is becoming the norm in new design. Boeing is jumping on the bandwagon and looking to win a major contract from NASA to create new subsonic/supersonic aircraft that will be more environmentally friendly. Concepts for the subsonic aircraft (noted as N+3 for the next three generations of aircraft) are all derived from the project known as SUGAR (Subsonic Ultra Green Aircraft Research). These include "SUGAR free" and "refined SUGAR" (I’m not making this up these puns) that resembles current 737 designs. SUGAR high and the electric/gas hybrid SUGAR Volt are more of a futuristic design and SUGAR ray (a design that looks like a B2 stealth converted for passengers) bringing up the rear. Finally, the SUGAR freeze (based on the SUGAR high) runs on cryogenically frozen liquid natural gas, making it 64% more efficient than current Boeing 737-800 planes.

 

All planes in this category have been designed to decrease CO2 emissions in one way or another; however the SUGAR Volt stands out from the pack because of its battery/fuel hybrid engines which reduce its energy burn by 55% over the other designs.

 


imageimageimage

 

(Left) refined SUGAR (Middle) SUGAR ray (Right) SUGAR high (concepts via Boeing)

 

The supersonic designs are just as diverse as their slower moving brothers that include a swing-wing configuration, a fixed-wing design that uses a ‘v-tail’ concept (called Icon 2) and a joined-wing ‘scissor’ (1 wing joined at the fuselage that rotates on a pivot point) concept. All the supersonic crafts are designed to lessen or reduce the inevitable sonic boom created with super-fast flight. Yes, Boeing understands that while the supersonic models aren’t exactly up-to-speed (as it were) on the whole green initiative, they more than make up for it in raw speed alone. Conceptual designs were also submitted by Northrop Grumman and Lockheed Martin to NASA as well, all in the hopes of winning a contract. If all goes according to plan, the first group of next generation planes will hit the runway in 2030.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • DAB
    DAB over 14 years ago

    Sugar is a hydrocarbon fuel with a lot of energy density.  After all, we humans use it.

    Not sure I am ready to sacrifice my chocolate habit so they can fly airplanes, but there are many new processes available for generating sugar compounds from a lot of materials.

    It still comes down to a cost and volume issue.  While it is technically green, there are a lot of costs involved with harvesting, converting the materials to sugar and then disposing of the by-products.

     

    I don't think these people have thought the whole lifecycle through.  I suspect that oil would need to cost about 1000 USD per barrel before this approach would be cost competitive.

     

    Just my opinion,

    DAB