Publications
  • Learn
  • More
Publications
Blog Solar film for windows, like a big sticker
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 10 Oct 2011 6:27 PM Date Created
  • Views 447 views
  • Likes 1 like
  • Comments 2 comments
  • alternative_energy
  • industry
  • cabeatwell:dit
  • energy
  • solar
  • innovation
Related
Recommended

Solar film for windows, like a big sticker

Catwell
Catwell
10 Oct 2011
image
CEATEC 3N solar film on curved glass. (Image via Tim Hornyak)
 
Almost every engineer I have ever met came up with this idea; a photovoltaic, solar, film that can be placed on window glass. However, for most of the people I know, financial constraints keep their ideas at bay. Luckily, mega-corp 3M had the time and money to make the idea come to fruition.
 
At the CEATEC, Combined Exhibition of Advanced Technologies, in Tokyo Japan, 3M unveiled the solar film which they called a "window transformative." The film is being pedaled as not only a solar generator but as an efficient heat-blocker absorbing 90% of infrared light, and also as a way to protect the glass from shattering. The film is glues to windows in large patches, like a giant sticker, and can even be placed on curved surfaces. 3M is also stating that anyone can install the solar film.
 
When it comes down to the true purpose of the film, solar-energy  generation, it is a bit of a letdown. At peak performance, the film only generates 20% of the energy a regular solar-cell can output. At the CEATEC event, 3M said that 1 square meter of the material can charge a cell phone during peak hours. 
 
Although the power output is low, the combined power output of a high rise covered in the film would be substantial. It is truly a step in the right direction. Now I get to hear all my associates say, "I had that idea." 
 
Cabe
  • Sign in to reply
  • Former Member
    Former Member over 14 years ago

    Creo que es un gran invento. Aunque el rendimiento sea bajo si el precio es suficientemente atractivo puede ser  muy atractivo para todo el Mundo. Desde Paises desarrollados hasta Paises subdesarrollados.

     

    ¿Cuando es el lazamiento del producto?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 14 years ago

    Even at 20% efficiency, when you multiply the square footage of glass around the world with at least some sun exposure, you can still generate gigawatts a day.  If they price the films for a reasonable amount, I would definately purchase them for my windows.  Every little bit helps, plus it is basically a one time expense with potentially decades of return on investment.

     

    Need to see the detailed numbers first though.

     

    DAB