Publications
  • Learn
  • More
Publications
Blog Super material graphene used to create laser pulses
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 4 Jun 2013 5:57 PM Date Created
  • Views 513 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • graphene
  • Design
  • cabeatwell
  • prototyping
  • university
  • innovation
  • communication
Related
Recommended

Super material graphene used to create laser pulses

Catwell
Catwell
4 Jun 2013

image

The honeycomb structure of graphene can soak up laser light, release it on command (via wiki)

 

Lately it seems that there is no applications in which graphene cannot be used to make a better product. It has already proved to be a superior material for conductors, solar cells, transistors, ultra-capacitors, and a variety of other applications. Now it appears scientists have just used graphene to produce ultra short laser pulses. In addition, scientists suggest that their experiments show that any color of light can be produced from these laser pulses.

 

In 2004, scientists discovered graphene. Five years later, physicist Andrea Ferrari from Cambridge showed that graphene can act as a source to absorb infrared light. Building on this finding, Ferrari along with other colleagues were able to produce experiments in which the graphene would release this light in ultra short pulses. These pulses, at the time limited to infrared light, were able to last up to a couple tens of femtoseconds.

 

Just recently, this work has been taken a step further. Their device has been improved to include a wide range of wavelengths it could produce. In addition, the scientists commented that due to the properties of graphene, it is theoretically possible to produce ultra short pulses over the whole range of the visible light spectrum. The applications of a laser that can produce different wavelengths of light can have the potential to create better products ranging from medical applications to micro-machinery.

 

Byung Hee Hong, a physcists at Seoul National University, commented, “In graphene, there is no band gap, and the electrons' energy can vary along a continuum. That gives the materials an advantage in fiber optics, enabling it to absorb a wide range of wavelengths of light. Usually, different materials are needed for different wavelengths, and there are not many materials that can be used for the near-infrared region.” Graphene's ability to absorb and produce light adds another feature to graphene's impressive resume. Band-gap was achieved with graphene. From that point alone, there are so many applications in which graphene holds an advantage. It’s only a matter of time before the tech hit the market and takes over. 

 

C

More news at

http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    Hi Cabe,

     

    Actually, I think it's the open atom structure of the graphene that enhances its absorbtion and emmission capabilities.

     

    The electron structure for the carbon atom is more open in the graphene structure.  Therefore more of the atoms are able to absorb the energy levels as it propagates through the atomic structure.

    The graphene lattice also helps to coordinate the photon emission as the energy flow along the electrons would facilitate the energy release points for the excited electrons.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    Hi Cabe,

     

    Actually, I think it's the open atom structure of the graphene that enhances its absorbtion and emmission capabilities.

     

    The electron structure for the carbon atom is more open in the graphene structure.  Therefore more of the atoms are able to absorb the energy levels as it propagates through the atomic structure.

    The graphene lattice also helps to coordinate the photon emission as the energy flow along the electrons would facilitate the energy release points for the excited electrons.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Catwell
    Catwell over 12 years ago in reply to DAB

    Thanks for the breakdown of graphene.

     

    I suppose we will all see graphene as a industry standard right when we need it. Right when depletion of the world's caches of standard electronic building materials. Go for the easy dollars before innovation...

     

    C