Publications
  • Learn
  • More
Publications
Blog Telepresence system lets users walk in a robot's shoes
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 29 Dec 2011 8:44 PM Date Created
  • Views 639 views
  • Likes 1 like
  • Comments 2 comments
  • haptic
  • test
  • transportation
  • hmi
  • tactile
  • telepresence
  • on_campus
  • eavesdropper
  • university
  • technology_for_the_disabled
  • sensor
  • innovation
Related
Recommended

Telepresence system lets users walk in a robot's shoes

Eavesdropper
Eavesdropper
29 Dec 2011
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


Humans being at two places at the same time may soon be analogous to humans flying. Dzmitry Tsetserukou and a team from Toyohashi University of Technology in Japan are working on making telepresence a possibility.
 
 
The system they are working on, NAVIgoid, will be unlike any joystick, mouse and keyboard controlled robot you have ever seen. The team has designed a belt with a four flex sensors and a 3-axis accelerometer that detects movements and allows the user to control NAVIgoid intuitively and precisely.  The belt can even detect the degree of bend or tilt of the torso to adjust the robots velocity just like a joystick.
 
 
One of the team’s main goals was to engage more senses than just vision. The NAVIgoid has two laser range finders (LRF) that scan all 360 degrees of its environment.  These LRF’s can detect the shape and the distance of still or moving objects. This information is then relayed to the wearable belt that has 16 vibration motors evenly placed around it. The motors can vary the intensity of vibration to provide high-resolution "vibrotactile" information to the user about the distance, direction, and even the shape of a still or moving obstacle.
 
 
This user feed back, along with visuals and sounds from the robot’s cameras and microphones, creates a stereoscopic image, which is wirelessly transferred to the head mounted display.
 
 
NAVIgoid currently has no arm or hand-like attachments. Since hands are not needed to control mobility, the team hopes to include apendages in later versions of the robot.
 
 
NAVIgoid was displayed at this years Siggraph Asia conference in Hong Kong.

 
See the latest on robot technology in the element14 Robotics group.

Eavesdropper
  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    Telepresence for medicine and dangerous occupations is at its beginnings.  We have the technology to make it happen and we will continue to see more implementations involving robots working where humans cannot.  Consider the untapped mining opportunities under the sea and on the moon.  The wealth of material available will indeed change the future as material acquisition costs go down and the hazards of mining and exploring diminish.

    Keep in mind, nearly 80% of the worlds surface is inaccessable by humans.

    We do not even know what we do not know about most of the planet.

     

    Think about it.

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 14 years ago in reply to DAB

    That is true. It must be easier to send vehicles to Mars that to the crushing depths of the ocean.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Catwell
    Catwell over 14 years ago in reply to DAB

    That is true. It must be easier to send vehicles to Mars that to the crushing depths of the ocean.

     

    Cabe