Publications
  • Learn
  • More
Publications
Blog The 9 nanometer carbon nanotube transistor
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 30 Jan 2012 8:18 PM Date Created
  • Views 915 views
  • Likes 1 like
  • Comments 1 comment
  • research
  • test
  • intel
  • transistor
  • industry
  • nanotube
  • 10nm
  • Design
  • cabeatwell
  • prototyping
  • measurement
  • ibm
  • innovation
  • 9nm
Related
Recommended

The 9 nanometer carbon nanotube transistor

Catwell
Catwell
30 Jan 2012
image
IBM carbon nanotube transistor concept drawing and performance (via IBM & NANO Letters)
 
"We are reaching the physical limits [of silicon]" - Aaron Franklin, researcher, at IBM Watson Research Center. What Franklin is predicting as an inevitable end, is 10 nanometers. At that point and below it becomes difficult to control a transistor. Intel's Ivy Bridge 3D transistor is about to reach that limit, but what happens then?

Franklin continued, "We've made nanotube transistors at aggressively scaled dimensions, and shown they are tremendously better than the best silicon devices." The team from IBM created a 9 nanometer carbon nanotube transistors. No transistor of its size can compete with the nanotube transistor's efficiency. The team placed the nanotube on top of an insulator, and connected the ends with electrical gates in a two-step process. The process ensured that the tube would not be damaged. The potential for a complete silicon replacement was demonstrated successfully. However, the tech does come with a set of challenges.


Making a pure batch of carbon nanotubes is the first issue. Placing, aligning, and connecting large numbers of these transistors is the biggest issue. As with all challenges, with enough time, money, and talent they will be toppled quickly. The future is one made of carbon.


Cabe
http://twitter.com/Cabe_e14
  • Sign in to reply
  • DAB
    DAB over 14 years ago

    The use of nanotubes in electronics is going to be the next big innovation.  I can't wait to see what they can do with more complex circuits using graphene and  other carbon based technics.

    I suspect we will soon see devices able to operate at the Terahertz level and consume very little powered.  At that level, you could see computers implanted in the human body using just your own body heat to power.

     

    Interesting possiblities.

     

    DAB