Publications
  • Learn
  • More
Publications
Blog The LEV-96 brings out the hidden harmonics in acoustic guitars
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 5 Nov 2012 6:52 PM Date Created
  • Views 597 views
  • Likes 0 likes
  • Comments 1 comment
  • research
  • moog
  • industry
  • guitar
  • hmi
  • cabeatwell
  • prototyping
  • sound
  • measurement
  • pickup
  • music
  • sensor
  • innovation
  • communication
Related
Recommended

The LEV-96 brings out the hidden harmonics in acoustic guitars

Catwell
Catwell
5 Nov 2012

imageimage

(Left) LEV-96 in the raw (Right) closer to production device (via MoogMusic)

 

Moog Music has been going strong since the early 50’s with products like theremin kits and Moog Modular synthesizer systems. Now they’re set to unveil the LEV-96 for acoustic guitars. According to Moog, the LEV-96 is a ‘sensoriactuator’ that is able to bring hidden harmonic/resonant frequencies (in this case from guitar strings) into the spectrum of human hearing from any ferromagnetic medium. Essentially, the device picks up the vibrational resonance from the strings that have previously been unheard but were nonetheless there all along. The LEV-96 was designed by placing 2 pick-up channels underneath each string which is able to control 8 harmonics per string resulting in a total of 96 harmonic resonances that can be handled at any given time. The harmonics are controlled by an onboard micro-processor (unknown as to which) and controlled through capacitive touch-based ‘sliders’ which can adjust the frequencies (harmonics, intensity and note sustainment). The device also has additional touch-based controls that provide additional settings such as tremolo, arpeggio and other various harmonic manipulations almost like using add-on effects pedals. The system settings are able to be locked so the player doesn’t inadvertently hit the controls while playing. Don’t get overly excited musicians, the LEV-96 is still being developed and is only in the working prototype stage. Chances are it will be ready for the consumer market sometime next year.

 

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • DAB
    DAB over 13 years ago

    I have been observing digital music for thirty years or so and there is still a distinct acoustic tonal quality from a real instrument over the synthesized ones.  The instrument itself in the hands of a master can generate very subtle additive sounds that the software just cannot duplicate.

     

    Yes the new devices are much improved, but you still cannot beat a live performance by talented people.

     

    Just my opinion,

    DAB