Publications
  • Learn
  • More
Publications
Blog TransOS, The first cloud operating system
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 18 Oct 2012 6:56 PM Date Created
  • Views 1510 views
  • Likes 1 like
  • Comments 3 comments
  • research
  • industry
  • hmi
  • cloud_os
  • telepresence
  • cell_phone
  • on_campus
  • cabeatwell
  • cloud
  • prototyping
  • operating_system
  • university
  • os
  • innovation
  • communication
Related
Recommended

TransOS, The first cloud operating system

Catwell
Catwell
18 Oct 2012

image

TansOS concept (via International Journal of Cloud Computing)

 

 

It is only an amount of time before cloud computing becomes the prominent method for storing and receiving data for your computers. Key advantages to cloud computing consist of automatic updates to software stored in the cloud, and access to all that is hosted in the cloud from any device with an internet connection. The next step in the cloud computing transition is to store the operating system that loads and runs all those applications and programs into the cloud, and its first incarnation is here.

 

 

Yaoxue Zhang and Yuezhi Zhou at Tsinghua University in Beijing China have developed the first cloud based operating system that they have dubbed TransOS.  Through use of a cloud OS, a bare-bones computer can access and run a full operating system downloading only TransOS code as needed. This can increase speed and functionality by keeping the memory free from running inactive system code such as in modern desktop computers. As a result, your computer essentially acts as a “dumb terminal,” which enables TransOS to work with low-powered computing and that switch between operating systems without hassle when they desire to.

 

 

In addition, the team working on the system also suggests that TransOS can allow devices other than computers to also access and operate TransOS. The concept helps bring the idea of the “internet of things” into better focus. Soon household devices such as washing machines and refrigerators along with mobile devices and cars will all have access to the cloud, and may possibly run through TransOS. The TransOS team has not made any official announcements for the release of  their product, although it is thought to be made available to the public early next year. More details of the system are scheduled to presented in the new issue of International Cloud Computing. 

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • DAB
    DAB over 13 years ago

    I would agree that most people may store and manipulate their data in the cloud.

     

    That said, there are still plenty of people, myself included, who still want to and need to control their data and its distribution.

    Some data are only of great interest to a few.  Even if I was offered a near perfect encryption storage, I would still retain and control my data.  Its that important to me.  No doubt, others will feel the same.

     

    I see the cloud as good and bad.  Yes it can be a benefit to those who like to share information, however, that data can be used by others for actions not necessarily benefiting the users of the Cloud.  Fears of 1984 coming true are still a likely possibility with the Cloud approach.

     

    Just my opinion,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 13 years ago

    I would agree that most people may store and manipulate their data in the cloud.

     

    That said, there are still plenty of people, myself included, who still want to and need to control their data and its distribution.

    Some data are only of great interest to a few.  Even if I was offered a near perfect encryption storage, I would still retain and control my data.  Its that important to me.  No doubt, others will feel the same.

     

    I see the cloud as good and bad.  Yes it can be a benefit to those who like to share information, however, that data can be used by others for actions not necessarily benefiting the users of the Cloud.  Fears of 1984 coming true are still a likely possibility with the Cloud approach.

     

    Just my opinion,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Catwell
    Catwell over 13 years ago in reply to DAB

    But a cloud OS could be powered my a computer system magnitudes more powerful than the latest buyable parts.

     

    People would no longer have to upgrade their computers or phones, it's done for them.

     

    C

    • Cancel
    • Vote Up 0 Vote Down