Publications
  • Learn
  • More
Publications
Blog Transparent graphene transistor material stretches beyond all others
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 11 Nov 2011 10:40 PM Date Created
  • Views 521 views
  • Likes 0 likes
  • Comments 0 comments
  • fabrication
  • graphene
  • transistor
  • on_campus
  • embedded
  • cabeatwell
  • prototyping
  • university
  • medical
  • material_science
  • innovation
Related
Recommended

Transparent graphene transistor material stretches beyond all others

Catwell
Catwell
11 Nov 2011
image
Final  graphene material (left). Magnified transistor image (center).  Transistors placed onto a balloon. (right) (Via Lee, American Chemical  Society)
 
There appears to be legions of engineers and scientists pushing hard for stretchable electronics.  The latest comes in the form of a transparent material containing sets  of graphene transistors. Up to a 5% flex could be achieved before  degradation of the electrical qualities.
 
In an effort that spans 10 schools, project lead Jeong Ho Cho from Soongsil University and Jong-Hyun Ahn from Sungkyunkwan University,  both are South Korea, found a way to overcome common issues with making  transparent and flexible electronics by using a different type of  substrate. In past attempts, a slab of rubber or balloon surface was  used with limited flexibility. Jeong and his team fabricated single  layers of graphene onto copper foil. Using photolithography and etching  tricks, the transistor components (electrodes, semiconducting channels)  were forced into the graphene layers. The etched graphene was  transferred to the clear rubber. A stretchable ion-gel was used in the  final step to finish the transistor's components, gate insulators and  electrodes.
 
Graphene  can  be printed at low, and even at room, temperatures. This gave the  team an easy way to make and manipulate the organic graphene. At the  same time, graphene's innate stretch ability was ultimately the key to  their success. The fabricated material could bend at a maximum of 5% for  1,000 flexes. After which micro-cracks started forming dues to  imperfections in the graphene layers.
 
As  most researchers will say, the team vows to improve the capabilities of  their transparent flex transistors. The team sees applications in  medical biosensores that form to the human body and flex  displays. 100%  flexibility is what they need, but that final 95% is always the  hardest.
 
 
Cabe
http://twitter.com/Cabe_e14
 
Although  the researchers are using graphene transistors, the actual operation of  which may be in question. The band-gap ratio for graphene is around 30.  The larger the band gap, the more of an insulator the material becomes.  For comparison, the band gap of silicon is 1.11.