Publications
  • Learn
  • More
Publications
Blog Universal Earphones detect which ear they are in, pumps music accordingly
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 3 Feb 2012 7:40 PM Date Created
  • Views 652 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • audio
  • industry
  • hmi
  • embedded
  • Design
  • prototyping
  • stereo_audio
  • music
  • sensor
  • innovation
  • communication
Related
Recommended

Universal Earphones detect which ear they are in, pumps music accordingly

Catwell
Catwell
3 Feb 2012

image

Universal Earphones (via Igarashi Design Interfaces Project team)

 

Another instance of "it is so simple it eluded me."
 
Designers from the Igarashi Design Interfaces Project, of the Japan Science and Technology Agency, have made a set of ear-bud style headphones that know which ear they are in. A proximity sensor built into each bud detects where the parts of the ear are located. The right ear will show up on one side of the sensor, left ear will be the other side. According to the picture, it looks as though it only senses one ear, where it will not sense the other at all, hence assuming "left." This detection allows the system to  deliver the stereo-audio channel accordingly.
 
The headphones also produce a "weak electrical current" through the user's head. This is used to detect when an ear bud is removed and shared with another person. Without the current signal, the system will immediately play the music/audio in mono. The goal is that when music is shared with another person, the fullest sound is delivered. This way both can hear all parts of the audio.
 
Extension of the project has its aim set on detecting when the buds are actually in the users ear via skin conduction sensing. That way the sound stream can be started or stopped automatically. The entire project will be showcased at the Intelligent User Interface Conference in Lisbon Portugal, February 14-17. More details as they come in during the show.
 
Cabe
http://twitter.com/Cabe_e14
  • Sign in to reply
  • Catwell
    Catwell over 14 years ago in reply to DAB

    Before I succumb to the our A.I. overlords, I would like to make my gadgets work harder for me.

     

    Another way to get the channels proper: This one is cruder, but would do the job easier. Manually press a button on either ear bud cord to indicate which channel is for the right ear. The system sets accordingly.

     

    More than one way to cook an egg.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 14 years ago

    Another neat idea that should have been found sooner.

    As our devices keep getting smarter, we may soon be at their mercy.

     

    Just a thought,

    DAB