Publications
  • Learn
  • More
Publications
Blog US Army and MIT develop fibre optic enhanced uniforms
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 20 Feb 2013 7:47 PM Date Created
  • Views 1207 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • defense
  • military
  • army
  • industry
  • hmi
  • uniform
  • on_campus
  • cabeatwell
  • prototyping
  • measurement
  • university
  • smart_material
  • sensor
  • innovation
  • communication
Related
Recommended

US Army and MIT develop fibre optic enhanced uniforms

Catwell
Catwell
20 Feb 2013

imageimage

(Left) The Battle Dress Uniform (BDU) in woodland camouflage. First issued in 1981 was replaced in 2008 with the (Right) Digital Army Combat Uniform. New smart-uniform may be the next generation. (via US Army)

 

The US Army has been known to develop some of the most advanced technology out in the world - the gear carrying Big Dog robot that walks or runs alongside army mates while withstanding any hit short of a missile is a testament to that statement. Now, through the Institute for Soldier Nanotechnologies venture, the Army and MIT are teaming up to provide soldier uniforms with a high-tech fashion upgrade.

 

 

The development of this project started a few years ago when Yoel Fink, a materials science professor at MIT, discovered that fibers used for fiberoptics could be fabricated out of a various assortment of materials through a process known as thermal drawing. Rather than sticking to the conventional glass filaments used in fiber optics, a composite fiber would allow fiber-operated devices to be built by choosing material strands with specific inherent properties.

 

 

Then, the idea to weave these compound fibers into an Army uniform to create a self-sensing and auto-communicating tech wear was engendered.

 

 

The goals for this project includes developing sensing fabrics that detect the outside environment to immediately localize threats and communicate with fellow soldiers, as well as enhancing the uniform to detect real-time physiological measurements of each soldier remotely. By combining a variety of materials, which include insulators, semiconductors, piezoelectric, acoustic transducers, and photo sensing technologies, a fully functional fiber is drawn and retrofitted to an Army uniform.

 

 

Both teams hope that the uniform upgrade will help bridge the communication gap that can be quite hectic on the battlefield. For instance, the technology can help inform other soldiers to the specifics of a wounded battle mate using the heat sensing fiber technologies. The tech would keep everyone linked and thus alert soldiers about incoming threats - the ultimate goal here being to save lives.

 

 

For now, the fiber-sensing uniform is at the prototype stage. The fabric, currently measuring 1 mm in diameter will need to be reduced to a size of about 100 microns before they will be thin enough for actual use. John Joannopoulos, the program’s director, plans to spend the next 10 years developing the technology. Hopefully by then, the tech won’t have a reason to be used on the battlefield, but it is nice to know that people are hard at work protecting the safety of our soldiers.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • Catwell
    Catwell over 13 years ago in reply to DAB

    The 1980s and wearable computer systems and sensors would appear science fiction.

    One person, from that era, said, "640k? Why would I need anything over 16?"

    It was a mindset not open to radical thinking.

     

    It only seems logical to monitor every aspect of our lives, especially the body.

     

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 13 years ago

    Its an interesting technology.

    When I suggested the development of something like this about 30 years ago, everyone said I was nuts.  Be that as it may, I am glad to see that others have seen the potential of building a personal monitor into the clothing.

     

    The utility of this technology goes far beyond military uses.  Anyone working in hazardous environments could benefit from this idea.  consider a coal miner, who needs to monitor methane levels, or people in the desert who need to monitor moisture loss, or even people working anywhere who get ill.  If you can detect these types of problems early, you can mitigate complications resulting from the issues you plan to monitor.

     

    In the sports world, you could actively keep track of the athletes physical condition during the competition.  You could greatly improve performance if you know when someone needs to be sat down for a bit to recuperate from over exertion or from a hard hit.

     

    There are a lot of health issues that could be detected and treated very early with this technology.

     

    I hope it quickly moves into the public apparal options.

     

    Lot of untapped potential here.

     

    Just my opinion,

    DAB