Publications
  • Learn
  • More
Publications
Blog US Army develops new way to squeeze more power from lithium batteries
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 11 Jun 2012 6:12 PM Date Created
  • Views 580 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • alternative_energy
  • test
  • lithium
  • on_campus
  • embedded
  • battery
  • cabeatwell
  • prototyping
  • measurement
  • university
  • energy
  • sensor
  • innovation
Related
Recommended

US Army develops new way to squeeze more power from lithium batteries

Catwell
Catwell
11 Jun 2012

image

Kang Xu, one of the people behind the innovation (US Army)

 

Researchers from the US Army Research Laboratory (ARL) have recently announced that they are able to generate more power from batteries through new design processes and materials. This small group of researchers are tasked with providing soldiers with power solutions that are both lightweight and energy efficient. Soldiers are being increasingly burdened with more technology everyday (communications, laser designators, NVG’s, etc.), and this requires them to carry a significant amount of batteries along with the 30 to 70Lbs worth of gear. The researchers developed their new lithium battery technology that provides 30% more power using what they call a ‘sacrificial additive’ that was developed a few years ago by US Army researchers Dr. Kang Xu and Dr. Arthur Cresce. The additive is an electrolyte made from a highly fluorinated phosphate ester structure. Their electrolyte additive bonds with the batteries cathode surface (carbonate-based electrolytes) which creates a stable interface that enables the battery to operate at 5 volts, which would be a first for single-cell battery solutions. The ARL researchers state that this new battery technology is just one advancement for the soldiers and that they’re looking towards the future with developments in ‘ubiquitous energy’ resources that would provide power through ‘indigenous sources’ such as making fuel from water (separating the hydrogen from water). Despite power saving schemes, the most popular operating voltage still sits at 5V. This battery will be welcomes with open arms.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • Catwell
    Catwell over 13 years ago in reply to DAB

    You have that right, on all points.

     

    Although 30% is a great boost, it will only increment the battery tech not revolutionize it. I believe that Lithium-silicon batteries are the future. (10 times the energy density)

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 13 years ago

    I like it, yet another great innovation coming out of the military research with instant application to the rest of the industry.

     

    I wonder how many people realize that we get about a 26:1 return on investment out of thes DARPA programs?

     

    Plus, who would have thought, batteries on drugs, you have to love the irony.

     

    DAB