Publications
  • Learn
  • More
Publications
Blog Virus Used to Convert Kinetic Energy to Electrical Current
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 1 Jun 2012 6:48 PM Date Created
  • Views 535 views
  • Likes 1 like
  • Comments 1 comment
  • research
  • alternative_energy
  • Design
  • cabeatwell
  • conversion
  • prototyping
  • university
  • medical
  • power
  • energy
  • innovation
Related
Recommended

Virus Used to Convert Kinetic Energy to Electrical Current

Catwell
Catwell
1 Jun 2012
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Walking down the street can one day help power our electronic gadgets. The idea may come true with a twist on the concept coming from a common virus. With a virus's unique traits and conservation of energy principles, researchers at Berkeley Labs have created the world's first organic piezoelectric material. A harmless virus is used to create electrical energy from mechanical energy and may one day be embedded into the sole of our shoes to charge our electric devices.

 

 

The research is still in the beginning stages, however, scientist have managed to assemble an electrical generator using an electrode coated with a specially engineered virus to power a LCD display. With the tap of a finger on the electrode, the force gets converted into electrical energy, and a small image appears on the LCD. The first applications of this research can lead to a paper thin generator that can be mounted onto moving objects or any object that experiences a force on a regular basis.

 

 

The driving effect used in the experiment is called piezoelectricity generated from the virus.  The M13 virus used is coated with helical proteins that release electrical energy when twisted and turned. To amplify this effect scientist added negatively charged particles to the outer layer of the virus which resulted in a larger potential energy output. The output of their LCD experiment yielded 6 nanoamps at 400 millivolts, just enough power to flash the number one on the LCD.

 

image

Test setup (via Berkely Labs)

 

Many piezoelectric devices are toxic making working with them difficult. However, the M13 virus is nontoxic and self-assembles into sheets. These properties make working with it to create small generators more simple than previous methods. We may soon be using small electrical generators during everyday tasks without even knowing it. The small films could possibly be connected to cars, doors, shoes, and bikes to help us save on our electric bills.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • DAB
    DAB over 13 years ago

    Hi Cabe,

     

    It will be interesting to see what kind of power densities they can achieve for each square inch of material.

    I could see a lot of use for these in survival suits, dive suits, hiking gear and just about any other physical activity.  You could use the power to support all kinds of devices.

     

    However, what happens if the virus mutates?

     

    Very interesting,

    DAB