Publications
  • Learn
  • More
Publications
Blog Wall riding robot uses jets
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 25 May 2011 6:36 PM Date Created
  • Views 885 views
  • Likes 2 likes
  • Comments 2 comments
  • research
  • dit
  • eavesdropper:dit
  • robotics
  • gripper
  • bernoulli
  • robot
  • on_campus
  • university
  • innovation
Related
Recommended

Wall riding robot uses jets

Eavesdropper
Eavesdropper
25 May 2011
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 
The University of Canterbury has created a new robotic locomotion across a vertical plane. The bot uses air to create a contactless suction force to hold the weight on any surface. It can even traverse gaps on walls as well. The method of hold is based on the Festo Bernoulli Gripper (FBG). Originally designed to transport solar wafers at high speeds during manufacturing, the FBG has minimal contact with the surface, leaves no residue, and is low-noise. The FBG forces air out fast enough to create a suction, lifting force, while allowing the entire device to glide on the forced out jets.

imageimage
 
With this bot, the FBG has been redesigned. To form a stronger type of jet, a 25 μm air outlet forces the air jets to push supersonics speeds, Mach 3 to be exact. This process allows for a FBG that is 5 times as strong as the conventional wafer moving counterpart, and still retains the low noise. Researchers claim their FBG will be available soon for around $100 USD.
 
Eavesdropper
  • Sign in to reply
  • Eavesdropper
    Eavesdropper over 15 years ago in reply to DAB

    I think surveillance might be the first use of non-manufacturing FBG style locomotion. I could see it as part of this military recon robot.

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 15 years ago

    This is really cool.  It is like a reverse air cushioned vehicle except it pulls the device into the surface instead of creating an air cushion to push it away.  I can see a lot of uses for this type of technology, especially for inspection, cleaning, or painting smooth surfaces.  It would make window cleaning much safer, you could paint water towers without climbing gear, clean ship hulls, man the list goes on and on.

     

    Well done.

     

    Thanks

    DAB