Publications
  • Learn
  • More
Publications
Blog Water flow generator using graphene
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 21 Jul 2011 5:59 PM Date Created
  • Views 651 views
  • Likes 1 like
  • Comments 3 comments
  • research
  • alternative_energy
  • dit
  • eavesdropper:dit
  • on_campus
  • university
  • energy
  • innovation
Related
Recommended

Water flow generator using graphene

Eavesdropper
Eavesdropper
21 Jul 2011
image
Graphene sheet, in blue, next to gold contacts (image courtesy of Rensselaer Polytechnic Institute)
 
To see how nanomaterials could be used to generate electricity from water flow, Rensselaer Polytechnic Institute professor Nikhil Koratkar has discovered the surprising potential of graphene as a generator. Using a sheet of graphene measuring 0.15mm by 0.03mm, Koratkar and his team observed the generation of 85 nano-watts. As water passes over the 1 atom thick graphene layer, chloride ions in the water stick the surface. As water continues to flow over the graphene, friction between the water and the absorbed chloride ions force the ions to drift in the direction of flow. These ion forces cause the free charges in the graphene to flow along the water's direction causing an internal current in the coating.
 
The immediate application for the discovery would be in hydrocarbon exploration. Koratkar stated that oil and gas companies want to increase the ease and efficiency of the search by using micro and nano-scale sensors sent into drilled wells to not only sense where they drilled but also laterally. The sensors would travel through underground water sources  to help uncover hidden pockets of oil and gas in the crevices of the earth. The sensors would be coated with a graphene layer, and as they travel through water they could generate their operating current.
 
Kptatkar explained, "It’s impossible to power these microsensors with conventional batteries, as the sensors are just too small. So we created a graphene coating that allows us to capture energy from the movement of water over the sensors... We’ll wrap the graphene coating around the sensor, and it will act as a ‘smart skin’ that serves as a nanofluidic power generator."
 
Further ideas for use, Koratkar mentioned self powered microbots and mico submarines, as well as coating the undersides of boats with a graphene layer. Keep in mind, 1 square millimeter of graphene could produce ~19 micro-watts in the presence of chlorine ions. How many square millimeters can you place on a aircraft carrier haul?
 
Eavesdropper
 
[The research team also tested carbon nanotubes in a similar fashion. The energy produced paled in comparison to graphene's output.]
  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    I can see using this same material in any place with dry air.  Think about all of the static electricity blowing in the wind!  You could set these collectors everywhere and generate just about all of the charge you could ever hope for.

     

    This Graphene stuff is starting to get really cool.  Its uses appear to be growing by the day.

     

    Thanks,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 14 years ago in reply to DAB

    I was interested to see if your idea would work.

    This tech works off the principle of molecules moving across the surface of the graphene. The molecular density of water is 1000 KG/m^3, and air is at 1.275 KG/m^3 at sea level. Air is 784 times less dense than water. In other words air would be 784 times less effective. That is only the case if the efficiency is linear.

     

    Until the graphene is more sensitive, we'll have to stick to wind turbines. Good idea though. Without proposing a question, we'll never get an answer.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Catwell
    Catwell over 14 years ago in reply to DAB

    I was interested to see if your idea would work.

    This tech works off the principle of molecules moving across the surface of the graphene. The molecular density of water is 1000 KG/m^3, and air is at 1.275 KG/m^3 at sea level. Air is 784 times less dense than water. In other words air would be 784 times less effective. That is only the case if the efficiency is linear.

     

    Until the graphene is more sensitive, we'll have to stick to wind turbines. Good idea though. Without proposing a question, we'll never get an answer.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • DAB
    DAB over 14 years ago in reply to Catwell

    Hi Cabe,

     

    The density issue is true, but I was thinking about the potential energy in the air that reaches hundreds of volts per metre.  If the Graphene can tap into that level of energy it may well be easier to extract more energy with less expense and risk from the air than you can achive with water.

     

    I think I will keep the air option open for now, there is clearly a potential there that has yet to be tapped.  That and Nicola Tesla was convinced that there was a way to tap into this planet wide power source and I still hold out hope that someone will learn what he knew and apply modern technology to the issue.

     

    Thanks,

    DAB