Publications
  • Learn
  • More
Publications
Blog WebOS is now open-source
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 9 Dec 2011 7:20 PM Date Created
  • Views 657 views
  • Likes 0 likes
  • Comments 4 comments
  • mobile_phone
  • hp
  • hmi
  • open_source
  • webos
  • embedded
  • cabeatwell
  • innovation
  • opensource
Related
Recommended

WebOS is now open-source

Catwell
Catwell
9 Dec 2011
imageimage
Logo and HP Veer with WebOS 2+ (via HP)
 

After the cancellation of all HP WebOS hardware, the future of the operating system looked bleak. Every HP statement implied their endeavor with the innovative mobile operating system was over.

 

The HP Pixi, Pre, and Touchpad all lost their luster in the public eye.

 

HP's new CEO, Meg Whitman, had the future of WebOS to contemplate as the first main bullet point to her new career choice. The community waited on bated breath for months, now the answer is here. WebOS is now being offered as open-source.

 

HP CEO Meg Whitman on her decision, "[WebOS] is the only platform designed from the ground up to be mobile, cloud-connected and scalable... By contributing this innovation, HP unleashes the creativity of the open source community to advance a new generation of applications and devices."

 

The ultimate goals were laid out as follows:

●  To accelerate the open development of the webOS platform

 

●  HP will be an active participant and investor in the project

 

●  Good, transparent and inclusive governance to avoid fragmentation

 

●  Software will be provided as a pure open source project

 

The application framework for webOS 3.0, ENYO, will also be offered up in the near future. Slowly but surely, every bit of the webOS user space will offered up for community “hacking.” If the widespread innovation over the open-source Android platform is any indication of where webOS may be headed, I am sure we will see the card interface on the most obscure mp3 players sometime soon. Luckily, a free-for-all fragmentation of webOS will be quelled; HP is retaining control over all related patents.

 

 

 

What can we expect? WebOS on more mobile hardware. More applications for the OS. A WebOS emulator for PCs. I, for one, cannot wait to start developing. Countless other feel the same way.

 

See a recent medical MRI app using a HP Touchpad and WebOS, after this link.

 

Cabe

http://twitter.com/Cabe_e14


 
Below is the email announcing the WebOS change from Meg Whitman to all of HP:
 
From: CEO – Meg Whitman
Sent: Friday, December 09, 2011 2:03 PM
Subject: webOS to be contributed to the open source community

Meg Whitman

CEO

TO/ All Employees


SUBJECT/ webOS to be contributed to the open source community


Today, we announced that HP will contribute our webOS software to the  open source community and support its development going forward. We  believe that this is the best way to ensure the benefits of webOS are  accessible to the largest possible ecosystem.


Since we announced the discontinuation of our webOS devices last  August, the executive team has been working to determine the best path  forward for this highly respected software. We looked at all the options  in the market today and we see a clear need for a platform that is both  open and has a single integrated stack.


webOS is the only platform designed from the ground up to be mobile,  cloud-connected, and scalable. By providing webOS to the open source  community and other hardware vendors we have the potential to  fundamentally change the landscape.


HP engineers, partners, other developers and hardware manufacturers  will be able to contribute to the development of webOS. Together, we  have an opportunity to make it the foundation of a new generation of  devices, applications and services to address the rapidly evolving  demands of both consumers and enterprises.


I would like to thank the webOS team for continuing your efforts under  very difficult circumstances during these last couple of months. Your  dedication is very much appreciated.


This is a very positive move for the development of our people, our software and HP overall.


We strongly believe that the best days for webOS are still ahead.


Best,


Meg
  • Sign in to reply
Parents
  • Sabrina
    Sabrina over 14 years ago

    As a long term Palm fan, current Pixi Plus and TouchPad owner, I do hope the community survives.  They do have a very strong dev group committed to WebOS so will be curious to see if there is any hope.  (A girl can dream, right?)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 14 years ago in reply to Sabrina

    Sabrina,

    Glad you are still using the Pixi. I have one too as a MP3 and video player, and have my Pre Plus (modded for Sprint) as a backup.

     

    HP announced they are supporting the the OS, and letting the open-source community do whatever they will for it. I would not consider this a death at all.

    Linux and Android are open source, and they seem to be doing well.

     

    I watched the palm employees slowly go at the webosnation.com blog. However, new people will fill in the void and bring with them, a new view and energy. Glad to see it.

     

    WebOS 3.0 was already ported to the HTC Evo 3D prior to going open source, foreshadowing possibility.

     

    Cabe

    http://twitter.com/Cabe_e14
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Catwell
    Catwell over 14 years ago in reply to Sabrina

    Sabrina,

    Glad you are still using the Pixi. I have one too as a MP3 and video player, and have my Pre Plus (modded for Sprint) as a backup.

     

    HP announced they are supporting the the OS, and letting the open-source community do whatever they will for it. I would not consider this a death at all.

    Linux and Android are open source, and they seem to be doing well.

     

    I watched the palm employees slowly go at the webosnation.com blog. However, new people will fill in the void and bring with them, a new view and energy. Glad to see it.

     

    WebOS 3.0 was already ported to the HTC Evo 3D prior to going open source, foreshadowing possibility.

     

    Cabe

    http://twitter.com/Cabe_e14