Publications
  • Learn
  • More
Publications
Blog Zigbee announces new Green Power feature with wireless energy harvesting
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 2 Jan 2013 7:45 PM Date Created
  • Views 951 views
  • Likes 0 likes
  • Comments 3 comments
  • research
  • alternative_energy
  • industry
  • power_management
  • cabeatwell
  • prototyping
  • wireless
  • power
  • energy
  • zigbee
  • innovation
  • communication
Related
Recommended

Zigbee announces new Green Power feature with wireless energy harvesting

Catwell
Catwell
2 Jan 2013

(2012 news)

 

image

Zigbee PRO Green concept image (via Zigbee)

 

 

The Zigbee Alliance (standard for high-level communication protocols) has just released their Pro Green Power feature (found in most smart metering systems) that not only allows for a wireless connection but harvests its own energy as well negating the need for a battery. The Pro Green feature set allows devices (including dimmers, sensors, switches etc.) without batteries to be securely integrated into Zigbee Pro networks. Essentially the devices are able to harvest widely untapped energy sources such as motion, light and vibration to power themselves without the aid of on-board or direct input power sources. For example flipping a light switch (that isn’t equipped with a battery) on or off that’s integrated on the Green Pro network harvests that energy which in-turn uses Zigbee protocols that turn on or off the corresponding light dedicated to that switch. The switch is active on the network (using 2 or more Green Power proxies on the same network) only for a short period of time to issue the on/off command until the small amount of energy generated is consumed (this makes the light switch essentially a ‘self-powered’ device). After which the switch will no longer appear on the Green Pro network. The new Pro Green feature allows the connected device to function using the harvested energy reliably, along with un-interrupting the network once the device ‘disappears’ when the energy has been expended. This will allow consumers and businesses to use Zigbee-related devices in areas where power connections are scarce, unavailable or prohibited due to the nature of the surroundings (some hospital areas, nature preserves or historical sites to name a few). So far a handful of companies have already adopted the Pro Green feature such as GreenPeak Technologies, which plan to use the feature in their RF-communication products including their upcoming release of their GP410 (IEEE 802.15.4 ZigBee PRO Green Power controller) chip.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • DaveYoung
    DaveYoung over 13 years ago in reply to DAB

    DAB, I totally agree that the energy harvested from a single flip of the switch can't be much -- Calculating 100% of the kinetic ennergy would be a good way to find the maximum theoretical energy available.

     

    However the goal may not just be focused on saving energy.  I wonder if there is a cost or size savings in harvesting the flip energy at low voltage, DC levels instead of having to make a power supply circuit to convert 120VAC to 3.3VDC. 

     

    In any case, I'd love to see their circuit in addition to the performance numbers that you're after.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 13 years ago in reply to DAB

    Depending on the environment, I am sure the harvesting is not as high as one would hope. But in an industrial location, wasted energy is everywhere.

    I am surprised that they are not trying to re-capture the wireless power being thrown everywhere. It must be far to little to be useful.

     

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 13 years ago

    I would like to see a well documented case study that can show the true energy savings using this approach.

     

    From a systems perspective I question the true "value" of this type of home automation.

     

    Just a thought,

    DAB