Publications
  • Learn
  • More
Publications
Documents Researchers Develop Technique to Remotely Control Cockroaches
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: squadMCU
  • Date Created: 7 Sep 2012 5:13 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 5:11 AM
  • Views 775 views
  • Likes 0 likes
  • Comments 1 comment
Related
Recommended

Researchers Develop Technique to Remotely Control Cockroaches

Researchers from North Carolina State University have developed a technique that uses an electronic interface to remotely control, or steer, cockroaches.

 

“Our aim was to determine whether we could create a wireless biological interface with cockroaches, which are robust and able to infiltrate small spaces,” says Alper Bozkurt, an assistant professor of electrical engineering at NC State and co-author of a paper on the work. “Ultimately, we think this will allow us to create a mobile web of smart sensors that uses cockroaches to collect and transmit information, such as finding survivors in a building that’s been destroyed by an earthquake.

 

“Building small-scale robots that can perform in such uncertain, dynamic conditions is enormously difficult,” Bozkurt says. “We decided to use biobotic cockroaches in place of robots, as designing robots at that scale is very challenging and cockroaches are experts at performing in such a hostile environment.”

 

But you can’t just put sensors on a cockroach. Researchers needed to find a cost-effective and electrically safe way to control the roaches, to ensure the roaches operate within defined parameters – such as a disaster site – and to steer the roaches to specific areas of interest.

 

The new technique developed by Bozkurt’s team works by embedding a low-cost, light-weight, commercially-available chip with a wireless receiver and transmitter onto each roach (they used Madagascar hissing cockroaches). Weighing 0.7 grams, the cockroach backpack also contains a microcontroller that monitors the interface between the implanted electrodes and the tissue to avoid potential neural damage. The microcontroller is wired to the roach’s antennae and cerci.

 

The cerci are sensory organs on the roach’s abdomen, which are normally used to detect movement in the air that could indicate a predator is approaching – causing the roach to scurry away. But the researchers use the wires attached to the cerci to spur the roach into motion. The roach thinks something is sneaking up behind it and moves forward.

 

The wires attached to the antennae serve as electronic reins, injecting small charges into the roach’s neural tissue. The charges trick the roach into thinking that the antennae are in contact with a physical barrier, which effectively steers them in the opposite direction.

 

In a recent experiment, the researchers were able to use the microcontroller to precisely steer the roaches along a line that curves in different directions. Video of the experiment can be seen here.

The paper, “Line Following Terrestrial Insect Biobots,” was presented Aug. 28 at the 34th Annual International Conference of the IEEE Engineering in Medicine & Biology Society in San Diego, Calif. The paper was authored by Tahmid Latif, a Ph.D. student at NC State, and co-authored by Bozkurt. Bozkurt has previously developed similar interfaces to steer moths, using implanted electronic backpacks.

  • cockroaches
  • to
  • control
  • remotely
  • researchers
  • technique
  • develop
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • derricknewark
    derricknewark over 14 years ago

    interesting application....

     

    Good thing insects have no pain receptors