Publications
  • Learn
  • More
Publications
Documents We're all talking about Wandboard!
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: DebuggerGuys
  • Date Created: 8 Oct 2012 10:51 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 5:14 AM
  • Views 829 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

We're all talking about Wandboard!

Wandboard

A new developer board with an ARM Cortex-A9 processor is due to hit the streets in November. It’s called the Wandboard, and it features a Freescale i.MX6 processor and a starting price of $69.


At that price, you get a version with a single core CPU and 512MB of RAM. If you need a little more power, you can opt for the Wandboard Dual which features a dual core version of Freescale’s processor and 1GB of RAM.


Both models feature w microSD card slots, HDMI and audio jacks, a SATA connector, and serial, USB, and Ethernet ports. But only the Wandboard Dual includes 802.11n WiFi and Bluetooth. You’ll need to plug in your own wireless dongles if you want WiFi or Bluetooth on the cheaper model.


Since this is a dev board, there are also GPIO pins which you can use to hook up additional hardware. The device also has an EDM connector, which should make it compatible with products that use the upcoming Embedded Design Module standard.


If you’ve noticed I haven’t mentioned anything about internal storage, that’s because there isn’t any. Like the Raspberry Pi, you use an SD card as the Wandboard’s primary storage. With two microSD card slots though, you can install the operating system on one card and leave it plugged in all the time, while using the other slot for removable storage.


As an ARM-based board, the Wandboard should be able to support Linux, Android, or other operating systems that can run on ARM chips. But the Wandboard developers say the software for this device won’t be available until mid-November when Freescale lifts the non-disclosure agreement on its i.MX6 software.

That’s also the time when the Wandboard will start shipping, but you can reserve one today at the Wandboard website.

  • board
  • wandboard
  • freescale
  • development_board
  • i.mx6
  • develop