Publications
  • Learn
  • More
Publications
Documents Cree unveils 'brightest lighting-class LED' (2)
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14news
  • Date Created: 25 Nov 2009 3:35 PM Date Created
  • Last Updated Last Updated: 12 Nov 2021 1:50 AM
  • Views 494 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Cree unveils 'brightest lighting-class LED' (2)

Cree has announced the release of a product which it claims is the brightest lighting--class LED on the market.

The company reported that the XLamp XP-G LED is now commercially available and could reduce the number of bulbs that a firm requires to light up an area.

Cree suggested that this could lead to financial savings, particularly since it claims that the LED has a high efficacy at a low current, which can reduce the amount of batteries or solar cells needed to operate them.

It explained that the product can produce 132 lumens per Watt (lm/W) at 350 mA, which can lower the power requirement for applications.

The firm, which recently won the top prize in the 2009 Lighting for Tomorrow - Solid State Lighting competition, also stated that the LED is the brightest in the industry, producing 367 lumens when powered by 1 A.

Due to producing efficacy of 111 lm/W, the bulb also creates a footprint that it 80 per cent smaller than the company's XR-E LED, while at the same time being 46 per cent brighter.ADNFCR-1785-ID-19478991-ADNFCR