Publications
  • Learn
  • More
Publications
Documents New high-temperature pressure sensor developed
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14news
  • Date Created: 15 Jan 2010 1:02 PM Date Created
  • Last Updated Last Updated: 7 Oct 2021 2:25 AM
  • Views 556 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

New high-temperature pressure sensor developed

A team of researchers have developed a pressure sensor that is able to withstand temperatures of up to 250 degrees C.

The average temperature that a pressure sensor can normally withstand is between 80 and 125 degrees C, but this was greatly improved by a team led by Dr Hoc Khiem Trieu at the Fraunhofer Institute for Microelectronic Circuits and Systerms in Duisburg.

He explained that the device has an additional layer of silicon oxide to better insulate it, which stops the item from leaking any current.

Dr Trieu said: "It prevents the leakage current that typically occurs at very high temperatures, which is the principal reason that conventional sensors fail when they reach a certain temperature."

Such sensors are often used by geologists when they drill into the earth to search for oil, with sensors required to withstand shocks and vibrations, as well as the high temperatures.

A recent study at the University of Southern California showed how a microelectromechanical system sensor can be used to distinguish between stable and unstable plaque in the body.ADNFCR-1785-ID-19559935-ADNFCR