Publications
  • Learn
  • More
Publications
Documents Production Programming by SuperPro Gang Programmers
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 25 Jun 2010 5:35 AM Date Created
  • Last Updated Last Updated: 7 Oct 2021 5:20 AM
  • Views 1954 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Production Programming by SuperPro Gang Programmers

imageSince SuperPro 5004 series gang  programmers have been launched in 2008, a new era has started for  universal gang programmers industry. The market has migrated from  conventional gang programmers design to faster speed, high technology  SuperPro production programming solutions. So what has changed with  SuperPro 5004 Gang programmers:

 

  1. For traditional gang programmers, all sockets controlled by one  processor and one data buffer which limits some important features  unlike SuperPro programmers provides.
  2. For traditional gang programmers, programming of chips is done  simultaneously but verifying is done sequentially. In other words, the 8  socket programmer may only provide 5 to 6 times the output instead of  8. But you get the full outcome out of SuperPro gang programmers with  its built-in RISC MCU.
  3. Xeltek gang programmers are equipped with 144-pin drivers by default  unlike other 48-pin gang programmers with limited device support.
  4. Xeltek gang programmers support over 58K devices by being the  industry leader as supporting largest device count. 60K device support  is around the corner.
  5. Asynchronous fast programming is ensured by each module being  independent from one another. The programming starts automatically when a  chip is inserted.
  6. With SuperPro 5004GP programming family, 1 Gb NAND Flash can be  programmer as low as 108 seconds.

 

Currently SuperPro  5004GP and SuperPro  5004EGP are listed as two of the gang programming solutions for  Xeltek's early 2010 product line. And these programmers are being highly  demanded by engineering workshops, IC manufacturing labs, programming  houses, etc...Basically any entity who is programming ICs in mass orders  are either considering to switch SuperPro or already using our  programmers.

 

What if 4 socket gang programmer is too much for your production  line, and one socket single programmer is not enough? Have you ever  heard of Clustered Programmers? With any stand-alone SuperPro  programmer, you can cluster and use it as a gang programming solution.

 

EspeciallySuperPro  501S 4-Cluster bundle is a preferred solution for this category.  What are the advantages of clustered programming:

 

  1. Start small and grow incrementally. You may start with 2 units and  add more units as the need grows.
  2. Clustering device programmers solution is based on operating in  PC-free (stand-alone) mode and does not require any PC screen operation,  and accordingly it minimizes the operator error.
  3. SuperPro Programmers can be operated by an inexperienced operator  with minimal training.
  4. It allows a person to easily operate 10 or more programmers  concurrently.
  5. Data security is maintained by removing the Compact Flash card at  the end of each operation.
  6. Service is easy. If a unit breaks down, the rest of the system is  still running while having the defective unit serviced.

 

Please take a look at the video where you can find demonstration of  how to cluster SuperPro 501S in stand-alone mode:

http://www.youtube.com/watch?v=EQVCwtUog6g

 

Since 2010, Xeltek has been offering SuperPro 5004GP, SuperPro  5004EGP, and SuperPro 501S 4-C as production programming solutions.  Considering the outcome, and the performance; SuperPro Gang Programmers  once again gives the highest value in return. Please do not hesitate to  contact us atsales@xeltek.com

  • xeltek
  • superpro
  • production_programming
  • gang_programmers