Publications
  • Learn
  • More
Publications
Documents Uniform organic LED lights could become a reality
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14news
  • Date Created: 19 Nov 2010 11:28 AM Date Created
  • Last Updated Last Updated: 7 Oct 2021 7:50 AM
  • Views 529 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Uniform organic LED lights could become a reality

Scientists working in Germany have announced a technique that could allow organic LED lights to emit more uniform illumination.

A team at the Fraunhofer Institute for Laser Technology, which specialises in developing lasers for applications such as cutting, welding and surface treatment, have used the devices to create better-conducting semiconductors for use in organic LED lights.

The reason why the luminaires typically do not offer great uniformity is because the indium tin oxide layer is not a strong conductor, meaning current cannot always reach the centre of the panel as well as it reaches the edges.

Now the team, led by project manager Christian Vedder, has established a technique which uses a mask to allow only very narrow strips of the indium tin oxide to be reached.

Conducting metal strips are melted through these slits using lasers, leaving a grid of very fine conductors on the surface of the layer that allows for better conductance and uniform light output.ADNFCR-1785-ID-800245826-ADNFCR