Publications
  • Learn
  • More
Publications
Documents im-PART-ing Knowledge, Understanding Component Engineering Series Part 2: Resistors
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: loucovey
  • Date Created: 28 Sep 2011 10:09 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 4:10 AM
  • Views 1936 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

im-PART-ing Knowledge, Understanding Component Engineering Series Part 2: Resistors

By Douglas Alexander and Brian Steeves, CE Consultants

Special to Footwasher Media

http://www.componentsengineering.com

 

My first up close and personal experience with a resistor was a 9V transistor radio in the middle of a Dodgers baseball game in 1959.

I was listening to the game in the fourth grade with the earphone wire snaked from my jeans' front pocket, through my belt, (first historical use of a strain relief), under my sweater, up through the button hole in my collar, (second historical use of a strain relief), to insert the plug end, inconspicuously, as close as possible to my inner ear, cleverly designed to avoid the teacher’s detection.

All of a sudden, I began to smell something burning. Then I lost the audio entirely. At recess, I opened the back of my transistor radio to discover a cylindrical device with colored stripes printed around the cylinder with one of the two red stripes partially obliterated by a brown-black burn site that extended to the board and wiped out the “R” before the 10 label. I missed the end of the game but I did catch the end of my radio. Thus, my first experience with troubleshooting had begun with my nose and had ended with my eyes. Later in life, I heard my electronics professor telling me that I had discovered the first two steps for troubleshooting any circuit.

From that point on, I have developed a long-term professional relationship with the resistor, the most commonly used discrete device in electronics.  The following is a discussion on some of the various resistor-based applications commonly in use today. This is not an exhaustive list, and the reader is invited to suggest other applications.

When placed in series with each other, with a tap connection between them, resistors are used as voltage dividers to produce a particular voltage from an input that is fixed or variable. This is one way to derive a bias voltage. The output voltage is proportional to that of the input and is usually smaller. Voltage dividers are useful for components that need to operate at a lesser voltage than that supplied by the input.

Resistors also help to filter signals used in oscillator circuits for video, audio, and many other clocked circuit devices. Used together with capacitors, this is known as an “RC” circuit, and the oscillation is a function of the two interacting to produce a time constant.

Because the flow of current through a resistor converts electrical energy into heat energy, the heat generated from the high resistance to the flow of the current is used commercially in the form of heating elements for irons, toasters, room heaters, electric stoves and ovens, dryers, coffee makers, and many other common household and industrial products. Similarly, it is the property of resistance that causes a filament to “glow” in light bulbs.

Current shunt resistors are low resistance precision resistors used to measure AC or DC electrical currents by the voltage drop those currents create across the resistance. Sometimes called an ammeter shunt, it is a type of current sensor.

Resistive power dividers or splitters have inherent characteristics that make them an excellent choice for certain applications, but unsuitable for others. In a lumped element divider, there is a 3dB loss in a simple two-way split. The loss numbers go up as the split count increases. Splitters can be used for both power and signal.

Resistors can be used in stepped configurations when they are tapped between multiple values or elements in a series. In the absence of a variable resistor (potentiometer), connecting to the various taps will allow for different fixed resistance values.

Using high-wattage wire-wound resistors as loads for 4-corner testing is a common practice in the qualification process of a power supply. By varying the line voltage and the resistive load to all four extremes, low line, high line, low load, and high load, a power supply’s operating limits can be determined.image

Wire-wound resistors (right), invented and patented by the African-American Engineer Otis Boykin, are also ideal for compensating strain-gauge transducers. They offer the necessary accuracy and perform reliably at high temperatures. They are designed to minimize resistance value change, or to change in a controlled manner over different temperatures. Wire-Wound resistors are made by winding a length of wire on an insulating core. They can dissipate large power levels compared to other types and can be made with extremely tight resistance tolerances and controlled temperature characteristics.

Typically, a single, one-megaohm resistor is used with an antistatic or ESD wrist strap for safely grounding a person working on very sensitive electronic components or equipment. The wrist strap is connected to ground through a coiled, retractable cable with the 1 mega ohm resistor in series with ground. This allows for any high-voltage charges or transients to leak through to ground, preventing a voltage buildup on the technician’s body and thereby avoiding a component-damaging shock hazard when working with low-voltage tolerance parts. This Transient Resistor, formula symbol is commonly referred to as a “mobile ohm”. image

These are usually designed in with a VoltsWagon pulling them. Can I get a groan from someone? Author’s note: This is not an original pun, but I would rather diode than young. Author’s note: That was original. Sorry, I just couldn’t resist—or could I?

Passive terminators consist of a simple resistor. There are two types: (1) a resistor between signal and ground like in Ethernet, or (2) a resistor pair, one from the positive rail to signal with another from the signal to negative rail. Terminating resistors are widely used in paired transmission lines to prevent signal reflection.

Impedance matching is the practice of designing the input impedance of an electrical load or the output impedance of its corresponding signal source in order to maximize the power transfer and/or minimize reflections from the load. Resistive impedance matches are easiest to design and can be achieved with a simple L pad consisting of only two resistors.

Fusible resistors, also known circuit protection resistors are designed with current limits in mind. When the current reaches a predetermined limit, the resistor opens like a fuse. This type of resistor would be used as a protection device.

Special Purpose resistors should be considered in this discussion, as well.

Memristor - a passive two-terminal electrical component in which there is a functional relationship between electric charge and magnetic flux linkage. When current flows in one direction through the device, the electrical resistance increases, and when current flows in the opposite direction, the resistance decreases. When the current is stopped, the component retains the last resistance that it had, and when the flow of charge starts again, the resistance value will be what it was when it was last active.

Varistor- (Voltage Dependent Resistor or VDR). A varistor’s function is to conduct significantly increased current when voltage is excessive.

Thermistor- type of resistor whose resistance varies significantly with temperature. Thermistors are widely used as temperature sensors, inrush current limiters, self-resetting overcurrent protectors, and self-regulating heating elements.

Humistor – Resistance varies with humidity

Ballast resistor - Another current limiting resistor, compensates for normal or incidental changes in the physical state of a system. It may be a fixed or variable resistor. Some ballast resistors are designed to increase resistance with an increase in current and, conversely, decrease resistance with a decrease in current.

Banister - The structure formed by uprights and a handrail at the side of a staircase – often used to resist falling...

By no means has this been an exhaustive discourse on resistor types or applications. Free documents with further detail on resistor technology with testing guidance, can be found here: http://www.componentsengineering.com/learning-center/components/passive-components/resistors.

  • impedence_matching
  • element14
  • varistor
  • electronics_industry
  • design_engineers
  • current_limiters
  • resistors
  • current-limits
  • ntp
  • passive_components
  • components_engineering
  • engineering
  • wire_wounddiscrete_components
  • current_shunt
  • electronics
  • circuit_protection
  • design_process