Publications
  • Learn
  • More
Publications
Documents ARM unveils world’s most efficient 32-bit processor
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: squadMCU
  • Date Created: 15 Mar 2012 8:17 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 4:49 AM
  • Views 730 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

ARM unveils world’s most efficient 32-bit processor

http://www.geek.com/wp-content/uploads/2012/03/Cortex-M0Plus_708-389x440.jpg

 

 

ARM has already made a name for itself by developing very efficient processors, and chances are you have a chip based on an ARM design inside your phone and/or tablet. But it’s not just the high-performance gadgets we use everyday that require processors, everything from home appliances to the vehicles we travel in and the medical equipment that monitors us contain a myriad of chips too.

 

Today, ARM has unveiled the world’s most energy efficient 32-bit processor, and it’s promising to open the way for many more very low power, always-connected devices and the so-called “Internet of Things.”

 

The new chip is called the ARM Cortex-M0+ and has a 32-bit architecture built using a 90nm process, which helps to keep costs down. As for power use, it consumes a mere 9µA/MHz while still managing to offer high-performance 32-bit processing.

 

Significantly, the M0+ offers both performance and power saving gains over the previous generation chip it the replaces: the Cortex-M0. But more importantly, ARM has developed a 32-bit processor that uses a third of the energy typical 8-bit and 16-bit processor require, while remaining competitive on price with those lesser chips.

 

Even though ARM is using a 90nm process for the M0+, it still manages to produce a chip that measures just 1mm x 1mm, and uses next to no power when in sleep mode. Depending on the device, when coupled with a battery pack this new chip could go years before the battery is depleted. It truly opens up a deploy-and-forget mentality for intelligent sensors.

 

Both Freescale and NXT have already licensed the Cortex-M0+, with Freescale confirming it has working silicon based on the design. It therefore shouldn’t take long before ARM’s latest processor starts shipping in products.

 

Read more at ARM Holdings

 

See Kinetis K seris

  • things
  • of
  • series
  • internet
  • world's
  • Processor
  • cortex-m0+
  • sensors
  • most
  • efficient
  • chip
  • freescale
  • kinetis
  • 32-bit
  • arm
  • k