Publications
  • Learn
  • More
Publications
Documents Chevrolet Cruze Now Available in the UK with New 1.7-liter Diesel that Returns up to 72.4mpg
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: iLOVEautomotive
  • Date Created: 17 Apr 2012 4:44 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 4:50 AM
  • Views 539 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Chevrolet Cruze Now Available in the UK with New 1.7-liter Diesel that Returns up to 72.4mpg

Chevrolet has announced the availability of a new and more frugal diesel engine for its UK market Cruze. The 1.7-liter VCDi unit will be offered on the five-door hatchback version of the Cruze starting in May and the newly revealed Station Wagon variant later this year.

 

image

 

The four-cylinder turbo diesel develops a maximum output of 128-horses (130PS) and a peak torque of 300Nm (221 lb-ft) accelerating the hatchback model from 0-60mph (96km/h) in 9.4 seconds and on to a top speed of 124mph (200km/h).

 

It returns a fuel economy of 51.3mpg UK in the city, 72.4mpg UK (3.9lt/100km or 60.3mpg US) on the highway and 62.7mpg UK (4.5lt/100km or 52.2mpg US) combined, with CO2 emissions of 117g/km.

 

Chevrolet UK Managing Director Mark Terry commented: "The new 1.7 VCDi gives Chevrolet a real opportunity to compete in the core area of the five-door hatchback market, where tax implications, fuel economy and CO2 emissions are critical."

 

The 1.7 VDCi will be offered in three trim levels on the Cruze Hatch including the entry-level LS, which is priced at £16,725 and comes with features such as air conditioning, ESC, remote central locking, follow-me-home headlamps, electrically-adjustable mirrors and electric front windows.

 

The mid-range LT is priced at £17,825, while the range topping LTZ at £18,685.

 

Via Carscoop

  • hatchback
  • CO2
  • diesel
  • economy
  • announcement
  • uk
  • automotive
  • four_cylinder
  • cars
  • chevrolet