Publications
  • Learn
  • More
Publications
Documents High Speed Travel Tubes Can Take You From NY To Beijing In 2 Hours
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: squadMCU
  • Date Created: 18 May 2012 9:04 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 4:52 AM
  • Views 610 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

High Speed Travel Tubes Can Take You From NY To Beijing In 2 Hours

http://cdn.elitedaily.com/elite/wp-content/uploads/2012/03/maglev-vacuum-train-11-485x306.jpg

 

The Evacuated Tube Transport (ETT) system would take   passengers from New York

to Beijing in just two hours. Advocates of Evacuated Tube Transport (ETT) claim it is

silent, cheaper than planes, trains, or cars and faster than jets.

 

How it would work:   put a  superconducting maglev  train in  evacuated  tubes, then accelerate

using linear electric motors until the design velocity is attained. Passive superconductors allow

the  capsules  to  float  in  the  tube,  while eddy currents induced in conducting materials drive

the  capsules.  Efficiency  of  such a system would be high,  as the  electric energy required to

accelerate a capsule could largely be recaptured as it slows.

 

http://cdn.elitedaily.com/elite/wp-content/uploads/2012/03/et3-system-2-454x400.jpg

 

The train capsules will be inserted and taken out of the tubes at “airlock stations

at  stations  along the routes.” The capsules are expected to be accelerated to a

velocity  of  4,000 mph;  after  they  reach  this peak, they will “coast through the

remainder  of  the  trip.”  Supposedly,  the tubes will be able to be networked like

freeways  but  will  need multiple tubes to keep from having scheduling delays on

long distance trips.

 

Capsules  can  be  made  large  enough  for  one  person  to travel or a large bus;

however,   the  ideal  capsule  size will be the same  as a car and carry four to six

passengers.The tubes will have more space than what is available on plane seats

for those who  worry about a claustrophobic situation.The passengers will also not

be able to feel  the speed at which they are traveling.

 

Even  if  this  way of traveling can seem a little daunting, if ETT were to become a

reality,   it  would  be  more  cost efficient, definitely faster, and much greener than

normal  travel.  It  is  also  suppose  to be an extremely safe way of traveling. ETT

travel  seems  very  appealing   and  could really improve the way that many things

are  delivered  other  than  people  such  as goods and medical supplies.  It will be

interesting to watch as this type of travel is  developed.

 

Source: EliteDaily.com

  • research
  • test
  • transportation
  • industry
  • prototyping
  • energy
  • solar
  • innovation
  • communication