Member and Staff Blogs Adjustable Bed for Laser Cutting
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 18 Mar 2020 11:50 PM Date Created
  • Views 2322 views
  • Likes 7 likes
  • Comments 8 comments
  • laser cutting
Related
Recommended

Adjustable Bed for Laser Cutting

ralphjy
ralphjy
18 Mar 2020

It feels a bit strange to be working on my projects in the midst of this Covid-19 crisis but since the advice is social distancing - I guess it is an appropriate activity.  Hopefully isolation will slow the rate at which the virus is spreading so that a mitigation strategy can be implemented.

 

I've been working on my low power (5.5W) laser setup that I've described in previous blogs.  I've recently been doing some lightweight cutting of 2.5mm thick craft wood.  I've been using a scrap 2"x4"x5" block of wood to cut against but I need something larger for general purpose cutting and also should use something that doesn't burn.

 

Here is the setup I've been using.  You can see the burn marks from cutting a square and also where I burned through when I was adjusting settings for engraving cardstock.

image

 

The bed of the CNC base is 7 inches deep and 12 inches wide so I got a 6"x12"x1/8" aluminum plate and drilled mounting holes at the corners.  I also used some 1/4-20 hardware and some springs so that I could have the capability to level the bed.  Here's the parts along with some guides that I printed to do material alignment.

image

And the finished assembly.

image

 

To provide a convenient way to make the leveling measurements I printed an adapter for a Digital Dial Indicator Gage to mount it to the spindle holder.

imageimage

image

 

I'd like to have a way to do the laser focus calibration automatically so I've considered buying the serial interface cable for the dial indicator but I want to see if I can use a mini Lidar time-of-flight sensor instead to do a non-contact measurement.  The absolute accuracy of the TOF sensor at 40mm is probably only 2mm but I'm hoping the measurement repeatability would be good enough to use for focusing.  I'd like the repeatability to be about +/- 0.25mm but I think +/- 0.5mm would be okay.  The other accuracy problem would be the reflectance of the material I'm cutting/engraving but it would be fun to give it a try.

  • Sign in to reply

Top Comments

  • ankur608
    ankur608 over 6 years ago +2
    Even, I have faced similar issues on 3018 Woodpecker (though I used it for PCB milling, hence solved through 'conductive feedback heightmapping' ). The Gauge-mod looks 'Perfect' on the machine.
  • Fred27
    Fred27 over 6 years ago +2
    I made a similar adjustable bed a while ago but used an aluminium honeycomb because I was doing more cutting than engraving. https://0xfred.wordpress.com/2013/02/22/laser-improvements-an-adjustable-honeycomb…
  • ralphjy
    ralphjy over 6 years ago in reply to Fred27 +2
    Thanks for the link to your project. I was hoping to find thicker rigid honeycomb that I could use - I think you are mainly cutting bigger pieces of material - maybe I am overly concerned with flatness…
  • Fred27
    Fred27 over 6 years ago +2
    The honeycomb is only really needed to draw smoke away from the rear when you're cutting and prevent reflections from marking the back of the work. It was very easy to cut as it's quite thin. It would…
  • ralphjy
    ralphjy over 6 years ago in reply to DAB +2
    Yes, the slotted bed was part of the CNC kit. This is a Sainsmart Genmitsu 3018-Pro. The kit was easy to assemble and I've been happy with it, but it is only good for lightweight applications which is…
  • dubbie
    dubbie over 6 years ago +1
    The idea of using a dial gauge is a good one and should provide a good ability to obtain perfect levelling. I know that on professional laser cutters that they use a thin wall cell/honeycomb structure…
  • ralphjy
    ralphjy over 6 years ago in reply to dubbie +1
    I agree with you and Fred that using an aluminum or steel honeycomb would probably be the proper way of doing this (especially with a higher power laser). I don't have the tools to do a good job of cutting…
  • DAB
    DAB over 6 years ago +1
    Very nice test. DAB PS, did the CNC bed come with the system?
  • Fred27
    Fred27 over 6 years ago

    I made a similar adjustable bed a while ago but used an aluminium honeycomb because I was doing more cutting than engraving.

    https://0xfred.wordpress.com/2013/02/22/laser-improvements-an-adjustable-honeycomb-table/

     

    The dial gauge is an interesting addition. I went with the simplest solution which was a piece of acrylic that was just the right side to slide between the cutting head and the workpiece when at the correct height. I know a common way to do this is a Dambuster's inspired technique of two laser pointers which align at the right height. This has the additional benefit of showing where your laser will cut/engrave.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago

    The idea of using a dial gauge is a good one and should provide a good ability to obtain perfect levelling.

     

    I know that on professional laser cutters that they use a thin wall cell/honeycomb structure as a bed for the material being cut, set in a water bed. I assume this is to minimised reflected laser light and to absorb heat. Does your aluminium plate reflect light? Get hot?

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ankur608
    ankur608 over 6 years ago

    Even, I have faced similar issues on 3018 Woodpecker (though I used it for PCB milling, hence solved through 'conductive feedback heightmapping' ).

    The Gauge-mod looks 'Perfect' on the machine.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<