Member and Staff Blogs Custom Trombone Kazoo Controller for Trombone Champ
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: thereminhero
  • Date Created: 5 Oct 2022 12:06 PM Date Created
  • Views 74294 views
  • Likes 8 likes
  • Comments 9 comments
  • controller
  • trombone
  • arduino nano
  • kazoo
  • tof sensor
Related
Recommended

Custom Trombone Kazoo Controller for Trombone Champ

thereminhero
thereminhero
5 Oct 2022
Custom Trombone Kazoo Controller for Trombone Champ

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

How it works

The Time-of-Flight (ToF) sensor measures the approximate distance between the main trombone section (bell brace) and the slider brace. It sends this data over USB Serial to the PC running my custom software, which combines this with audio data from the microphone. The mouse is then moved relative to the changing distance from the sensor, and clicked whenever a loud sound is heard. The click is held for the duration of the sound. In other words, the audio pitch doesn't matter, just the volume. It's up to your accuracy with the trombone slider to nail the notes! 

Hardware

Components used:

  • Trombone Kazoo
  • Arduino Nano
  • VL53L1X Time-of-Flight (ToF) sensor
  • Microphone attached to computer running the game (any will do)

Tools needed:

  • Soldering iron + solder
  • Hot Glue

imageimage

Software

The latest windows software release and Arduino sketch can be found on my GitHub

To build the arduino sketch you will need to use the Arduino Library Manager to install the VL53L1X Pololu library - I used v1.3.1

Game Configuration

  • Ensure that the game is configured in windowed mode so that the audio monitor can be seen.
  • Run the audio delay compensation calibration
  • Enable inverse mode
  • Increase the mouse sensitivity (2x or higher)
  • You will need to adjust the starting position of the mouse for every song to ensure the full range of motion is available
  • Use the 'm' key to toggle mouse control on or off - this works even if the control software is in the background

Controller Configuration

  • You can change the calibration of the controller further with the Configure button
  • It lets you switch COM ports if you have multiple
  • It lets you switch between ASIO and Windows default driver for the audio capture (this might be buggy at the moment, later versions will be more stable)
  • Make sure to set your default mic in windows to the one you want to use
  • Sign in to reply
Parents
  • dereksalright
    dereksalright over 2 years ago

    Hi! I have zero knowledge and experience with any of this at all, but I love Trombone Champ and would love to try this out!

    I have all the tools and hardware, and I've downloaded and installed the latest Windows version of the Trombone Controller software.

    I have Arduino IDE installed, and successfully uploaded the sketch to the Arduino Nano.

    I have the Trombone Controller up and running, Port is on the correct Port, mic is hooked up and looks to be affecting the green/red bar, game is running, but the mic doesn't seem to register as mouse clicks and the sensor isn't controlling the mouse at all. Any advice?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • thereminhero
    thereminhero over 2 years ago in reply to dereksalright

    You will need to use the Arduino Library Manager to install the VL53L1X Pololu library - I used v1.3.1. Then it should build. I've updated the post to include this info.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dereksalright
    dereksalright over 2 years ago in reply to thereminhero

    Thank you for the swift reply! I now realize I got the wrong sensor (I bought the "VL53L0/1XV2" instead of "VL53L1X"-- that's what I get for blindly searching for it on Amazon hah) so I've ordered the exact Pololu VL53L1X. Will update here when it arrives! Thanks again for checking in, ThereminHero!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dereksalright
    dereksalright over 2 years ago in reply to thereminhero

    Thank you for the swift reply! I now realize I got the wrong sensor (I bought the "VL53L0/1XV2" instead of "VL53L1X"-- that's what I get for blindly searching for it on Amazon hah) so I've ordered the exact Pololu VL53L1X. Will update here when it arrives! Thanks again for checking in, ThereminHero!