Member and Staff Blogs Desoldering Tip When Nothing is Working For You
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Sean_Miller
  • Date Created: 22 Jul 2019 9:00 PM Date Created
  • Views 4128 views
  • Likes 12 likes
  • Comments 9 comments
  • ps4 hdmi
  • desoldering
Related
Recommended

Desoldering Tip When Nothing is Working For You

Sean_Miller
Sean_Miller
22 Jul 2019

This blog is written to help me remember this trick.  I'm sure its actually a common approach, but it just wasn't an approach I've bumped into.

Original issue:  PS4 HDMI Port Failure

 

The HDMI port of my son's 5 year old PS4 had a couple of bent pins that would push back into the unit.  In turn, it had no display.  I found a replacement port for just 5 bucks, so I decided to give it a try versus scraping the unit.

 

Removal of the Port:

I removed the port by snipping its 4 mount pins.  I then used a bench top heated air blower to remove it.  This went well until I went to remove the 4 mounts pins.

 

My SMD soldering rework station at its max setting of 500F wouldn't melt the solder.

 

My soldering iron at 850F wouldn't melt the solder.

 

I tried flux and attempting to add more solder to get the old to flow, but it didn't work.

The Solution:

After a lot of head scratching, I decided to try my Porter Cable 1500W heat gun with an accessory tip that took the air stream to 1/2".  Although I couldn't find this guns max temperature, I found a source online that claimed most guns run at 1150F.  This gun is typically for removing paint or heating heat shrink.  However, it did the trick to desolder those mount pins.

 

Taking care not to cause collateral damage, I pointed the air flow at one pin at a time on the max temp/flow setting.  The solder quickly went shiny.  With the other hand, I used tweezers to snatch out the mount pins.

The Conclusion:

Had I known the gun was an option, I would have used it instead of cutting the mounts pins in the first place.  This would have evenly heated the boards pin for the entire port's contact points.

 

Also, when you purchase a hot air rework station, get the highest wattage you can.  But, if you get in a pinch, you can use your hot air gun successfully.

 

-Sean

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 7 years ago +8
    Most likely the pins were soldered to the big ground plane. 500°F (260° C) is on the low side for unleaded solder. And the pencil may not have had the capacity to keep the heat with that ground plane involved
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to dougw +5
    I bought a cheapie hot air station when I was just experimenting with a repair of a board. I found it does fine with mounting SMDs with solder paste or removing smd components. With this motherboard, it…
  • koudelad
    koudelad over 7 years ago +5
    I used a hobby hot air gun to remove a rotated 48-pin TQFP in my IR thermometer build and it went OK (the chip still works after this rework). Temperature regulation is sometimes useless, if the device…
  • dougw
    dougw over 7 years ago +4
    I'm surprised your hot air doesn't go higher. I think my Aoyue goes to 900 degrees, especially when the air flow rate is reduced, although I don't ever run that high as it can damage the PCB at that temperature…
  • jw0752
    jw0752 over 7 years ago +4
    Hi Sean, I use a 260 watt Weller gun for these situations. I allow the tip to get quite hot and then I hit the point I want to desolder. The very hot tip melts the solder before the copper ground plane…
  • jw0752
    jw0752 over 7 years ago in reply to Sean_Miller +3
    Hi Sean, You won't regret the Weller. I build a lot of structures and brackets out of 12 Ga copper wire and the Weller is great for soldering joints. . Here is a battery bracket that was soldered with…
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to jw0752 +1
    I took a look and found my soldering station is only 70W (Weller WE1010). That 260W sounds like a beast that definitely would do the trick. I do like the precision of using a tip over air. I might need…
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to jw0752 +1
    Well...I bought a Weller gun. Bought their highest wattage gun on the market. It should be here in a few days. As expected, getting those mounts to solder back on just didn't work. I did the heat gun trick…
Parents
  • koudelad
    koudelad over 7 years ago

    I used a hobby hot air gun to remove a rotated 48-pin TQFP in my IR thermometer build and it went OK (the chip still works after this rework). Temperature regulation is sometimes useless, if the device has no feedback regulation. I had no idea about the target temperature, but you can see the start of melting the alloy. The only way was to approach to the chip slowly and regulate the target spot temperature by the distance to target.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • koudelad
    koudelad over 7 years ago

    I used a hobby hot air gun to remove a rotated 48-pin TQFP in my IR thermometer build and it went OK (the chip still works after this rework). Temperature regulation is sometimes useless, if the device has no feedback regulation. I had no idea about the target temperature, but you can see the start of melting the alloy. The only way was to approach to the chip slowly and regulate the target spot temperature by the distance to target.

    • Cancel
    • Vote Up +5 Vote Down