Member and Staff Blogs Forgotten treasure
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: gecoz
  • Date Created: 21 Feb 2019 6:02 PM Date Created
  • Views 1838 views
  • Likes 16 likes
  • Comments 14 comments
  • vintage
  • valves
  • radio
  • magnadyne a 30
Related
Recommended

Forgotten treasure

gecoz
gecoz
21 Feb 2019

I can still remember when, more than 4 decades ago, I was used to go and visit my grandmother Vincenza at her place for every holiday. It was never a long stay, just a day trip, as she lived in Nettuno, near Anzio (famous for the landing of the Allied forces during the second World War), about an hour away from Rome, where I was born. We would arrive usually mid morning.

 

There were a few hunches that would make you immediately realise that was my grandma's home: the first was the lovely smell of a meat bases tomato sauce, slowly cooking on the hob in the kitchen, that would fill the whole house. The second was the gentle noise of a radio playing in the background. It was like a magnet to me: I always loved to sit and tune the radio, while staring with amazement at the magic eye's green florescent beam, widening and narrowing as you fine tuned to the station.

 

When my  grandmother passed away, nearly 4 decades ago, I knew what I would have loved to keep, as memory: her gorgeous radio! It was a Magnadyne ANIE series, 5-valve + 1 magic-eye valve, 1 Medium waves band, 2 Short waves bands, produced in Turin, Italy in the 1950's. When I got it, it was still in good working order, and I even managed to get some spare valves, in case one would blow.

 

This week I have been travelling back to Rome, and managed to visit my mum. After long time, I decided it was time to get the radio down from its shelf and try it out.

 

image

 

I wasn't very confident about being even able to power it on, after all the time spent just gathering dust. So, armed with a cloth, I got it down and started dusting it. The wood is still in very good condition, and so the plastic on the front. The knobs have an outer and an inner control each: the left one has the volume control on the outer and the tone control on the inner. The right knob has the tuning control on the outer ring, and the inner control is a multi-position switch, for the band selection.

 

It is time to remove the back cover, and have a look (after a good dusting!) at the inside of this beauty.

 

image

 

The first thing you notice is the 5 valves, lined up on the metal chassis, and the magic-eye valve attached on the front wood panel. It strikes the cleanness of the design and the arrangement of the components. Besides the valves, it is easy to spot the variable capacitor used for the tuning circuit, on the left, the transformer for the power supply, on the right, Unfortunately, to gain access to the bulk of the circuitry, I would have had to dismantle the radio completely, as they sit just underneath the metal, and I have not got any tool here with me to do it safely, without risking to damage the radio.

 

image

image

image

 

After a rapid inspection, I decided to power on the radio. I cannot see any sign of damages, with exception of what I believe is a capacitor with a false contact on the tone control potentiometer, which should affect only the quality of the sound.

 

Used to immediate response of nowadays electrical appliances, it felt like a very very long time from the moment I turned the switch on to the moment some sound started coming out the speaker. But valves need time to warm up, before the circuit starts behaving properly. And you can visually witness the warming up, by looking at the valves and look at them starting to glow. Unfortunately, one thing I noticed straight away is the failure of the magic-eye: no green glow is showing.

 

Not having any schematics available, I can only guess what the cause could be. The valve itself doesn't look damaged, so the next suspect would be another faulty contact. Again, to try and trace it, I would need to strip the radio, so I will just have to live with this for now.

 

image

image

 

Finally, I'm doing what I was used to, many many years ago: scan for a station to tune in. Unlike the last time I tried it, I don't seem to get any luck tuning into any station. After slowing turning the control and try scanning all the bands, I finally manage to get a very feeble signal (in the video you probably you can just ear it, immersed in loads of noise!) from a station in the medium wave band.

 

I suspect the cause of this degradation of the performance is due to the obsolescence of the component (I spotted quite a few electrolytic capacitors when I peeped under the metal case).For now, I will not try and attempt a replacement of components, to fix the problems, and it seems I managed to misplace the replacement valves I had. I'm sure they will be somewhere in the house, and will probably pop up next time I will be visiting my mum!

 

I'm pleased that, in general, this old friend is still "alive", but even if it had stopped working, it would not stop bringing up the memories of all the nice times spent with it, and all the memorable dinners had at my grandmas!

 

Thanks for reading.

 

Fabio.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 7 years ago +11
    Hi Fabio, It was nice to read the history of the radio, and it has been kept safely, the front panel also still looks really great! Here is the schematic:
  • DAB
    DAB over 7 years ago +9
    Hi Fabio, Great post. Try moving the valves (aka tubes) in their sockets. They sometime oxidize, which alters the connections. From the sound of the audio, I would say you might need to replace some of…
  • gecoz
    gecoz over 7 years ago in reply to 14rhb +8
    Hi Rod, Thanks for your comment. Indeed, I too hope to be able to restore it to its former glory. Ideally I would have to bring it back with me to the UK, but I don't see it happening, as I would not trust…
  • jw0752
    jw0752 over 7 years ago +8
    Hi Fabio, Thanks for this great post and my own memories that it triggers. Like you my Grandmother had a radio that played Polka music every morning as she worked to make breakfast for the men returning…
  • 14rhb
    14rhb over 7 years ago +7
    Hi Fabio, A truely fantastic piece of vintage tech and it sounds like you have some great memories of it. Thanks for sharing the photos. Hopefully in time you'll get the components you believe have deteriorated…
  • genebren
    genebren over 7 years ago +6
    Great to have your fond memories intact and faced with the opportunity to do a restoration on a great piece of vintage gear. Gene
  • gecoz
    gecoz over 7 years ago in reply to DAB +5
    Hi DAB, Thanks for your advice. While dusting off the components, I removed all the valves from their sockets. I didn't clean the contacts though. I agree, the capacitors will need replacing. Hopefully…
  • gecoz
    gecoz over 7 years ago in reply to jw0752 +5
    Hi John, It is amazing how some things can carry such value, and bring back so many memories and emotions. Your Grandma's radio still sounds great, you can tell it has been much loved! Thanks for sharing…
  • fmilburn
    fmilburn over 7 years ago in reply to jw0752 +5
    I think we had the same exact radio as yours John when I was young. Alas, it disappeared in the 60s when my parents bought a stereo console complete with record player and radio.
  • gecoz
    gecoz over 7 years ago in reply to shabaz +4
    Hi Shabaz, That's great, thank you for the schematic. Fabio
Parents
  • 14rhb
    14rhb over 7 years ago

    Hi Fabio,

     

    A truely fantastic piece of vintage tech and it sounds like you have some great memories of it. Thanks for sharing the photos. Hopefully in time you'll get the components you believe have deteriorated back and working.

     

    Rod

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • 14rhb
    14rhb over 7 years ago

    Hi Fabio,

     

    A truely fantastic piece of vintage tech and it sounds like you have some great memories of it. Thanks for sharing the photos. Hopefully in time you'll get the components you believe have deteriorated back and working.

     

    Rod

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • gecoz
    gecoz over 7 years ago in reply to 14rhb

    Hi Rod,

     

    Thanks for your comment.

     

    Indeed, I too hope to be able to restore it to its former glory. Ideally I would have to bring it back with me to the UK, but I don't see it happening, as I would not trust the radio with any of the airlines, judging by the state of my luggage after any trip!

     

    So, the other way is to do a bit at time, every time I'm back visiting in Rome, but I will have to get some tools. Finding the schematics will be a challenge in itself... I might have to resort to retrace the circuit just by looking at the connection, once I will strip the radio.

     

    I think it might become a project for when I retire... image

     

    Fabio

    • Cancel
    • Vote Up +8 Vote Down