Member and Staff Blogs need help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ezain
  • Date Created: 15 Nov 2026 12:17 PM Date Created
  • Views 37 views
  • Likes 2 likes
  • Comments 2 comments
  • pcb
  • help_required
Related
Recommended

need help

ezain
ezain
15 Nov 2026

dear engineers,

I am a 15-year-old starting out with PCB design. I recently designed a continuity tester circuit to check if a wire is properly connected or two pieces of wire are properly connected together. I built the circuit using an A1357 PNP transistor, a 10,000 Ω resistor, and some other components. The first picture shows my circuit schematics and the second picture shows the final version, now 

my circuit exactly follows the schematic and I checked it with another continuity tester. All the connections seem to be fine but the problem is that when I try to use the circuit, it does not work.

I have tried rewiring it and refreshing the solder in case there were any cold solder joints but it looks like my circuit wiring is fine. It could be an issue with the transistor since the transistor was very old. I want your help to figure out if there is something wrong with my schematics or if there can be another issue with it.

Your help will be highly appreciated,by a young hobbyist 

 now I know that  I was supposed to put a resistor before the LED since I'm using 9 V but when making the circuit I completely forgot the resistor. That does not matter because my LED was in parallel with my buzzer. Even if the LED does not work, in parallel circuits the other component always works 
image

image

image

  • Sign in to reply

Top Comments

  • shabaz
    shabaz 17 hours ago +1
    Hi, That circuit is not convenient to follow, there are at conventions for drawing circuits: (1) High voltage at the top, low voltage at the bottom (2) Inputs on left, outputs on right. The circuit…
Parents
  • shabaz
    shabaz 17 hours ago

    Hi,

    That circuit is not convenient to follow, there are at conventions for drawing circuits:

    (1) High voltage at the top, low voltage at the bottom

    (2) Inputs on left, outputs on right.

    The circuit here may work (you may still need to tweak it, but it will provide you with results you can move forward with so I'd strongly suggest just restarting and putting your current circuit to one side, maybe desolder the parts and reuse.

    image

    Better to test without the buzzer, just the LED, and then add the buzzer once you have confirmed it works with the LED.

    You mention you forgot the LED resistor, but it's essential, you won't get expected results if it is missing.

    The values you can adjust, if you don't have the same values as the ones in the diagram. For example, R1 can be anything between 470 ohm and 10 kohm. R2 can be from 47 kohm to 470 kohm. R3 can be from 1 kohm to 10 kohm.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ezain
    ezain 4 hours ago in reply to shabaz

    Thankyou for your help (sorry if you had to put effort into it) I will now test this curcuit in my breadborad then remake the whole curcuit, hope it works just fine this time Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ezain
    ezain 4 hours ago in reply to shabaz

    Thankyou for your help (sorry if you had to put effort into it) I will now test this curcuit in my breadborad then remake the whole curcuit, hope it works just fine this time Slight smile