• Products and Partners
    Products and Partners
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
Member and Staff Blogs Programming Python on Xilinx Zynq
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: alexwonglik1
  • Date Created: 4 Apr 2018 10:58 PM Date Created
  • Views 1829 views
  • Likes 9 likes
  • Comments 4 comments
  • python
  • xilinx
  • fpgafeatured
  • fpga development kit
  • fpga
  • hackster.io
  • digilent
  • xilinx zynq
  • fpga dev
  • xilinx;
  • vivado design suite
  • python&linux
Related
Recommended

Programming Python on Xilinx Zynq

alexwonglik1
alexwonglik1
4 Apr 2018

Python is a very powerful and flexible programming language, enabling engineers to perform complex mathematics analysis, implement Artificial Intelligence solutions and develop a range of other complex engineering solutions. The ability to use Python within the Field Programmable Gate Array (FPGA) space has however previously been limited. With the release of the PYNQ framework, Python developers for the first-time were able to exploit the capabilities and performance provided by programmable logic. FPGA developers also benefited as they were able to integrate the high-level capabilities of Python with their FPGA designs. A recent project on Hackster.io by Adam Taylor exemplifies how one can combine this powerful hardware and Python for the implementation of their ideas.

 

To get started with the tutorial, one can pick up Digilent Arty 27-20 as well as a MicroSD card (which should be at least 8 GB if possible). The first step involves getting the PYNQ image up and running on the Digilent Arty 27-20. Once this is complete, the ISO File should be burned to the MicroSD card. Once these steps are complete, it's time to insert the micro SDcard into the Arty Z7-20. If things run smoothly, you will see the Done LED illuminate, indicating the Xilinx Zynq has been configured, followed by activity on the Ethernet LEDs. Once the boot sequence is complete and the PYNQ framework is ready. The four LEDs and two RGB LEDs will flash several times before leaving the four LEDs illuminated.

 

imageimage

 

Next the tutorial goes into depth about how to leverage Python on the Arty Z7-20 by using Jupyter notebooks.

 

image

 

In addition to getting you started with utilizing the PYNQ framework the tutorial goes into depth on how the programmable logic can be used to provide several interfaces and programmable logic overlays. This includes developing custom overlays, which can be done in either Vivado Design Suite including SDK and High-Level Synthesis using Vivado HLS or SDSoC Development Environmen so users can fully harness the power of both Python and FPGA.

 

image

  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +2
    Nice update. I like the idea of running Python on the FPGA. I will keep this idea in mind. DAB
  • stårkkkk
    stårkkkk over 6 years ago +1
    can normal python program can be run on this xilinx fpga??
Parents
  • DAB
    DAB over 8 years ago

    Nice update.

     

    I like the idea of running Python on the FPGA.

     

    I will keep this idea in mind.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 8 years ago

    Nice update.

     

    I like the idea of running Python on the FPGA.

     

    I will keep this idea in mind.

     

    DAB