Member and Staff Blogs Raspberry Pi BLE and WiFi Internet Radio - Part 3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 4 Jul 2022 3:16 AM Date Created
  • Views 13402 views
  • Likes 13 likes
  • Comments 12 comments
  • ble
  • wifi
  • radio
  • raspberry pi
  • moode
  • internet radio
  • streaming
Related
Recommended

Raspberry Pi BLE and WiFi Internet Radio - Part 3

fmilburn
fmilburn
4 Jul 2022

This is an update of the Raspberry Pi Internet Radio project I’m doing with my brother.  My brother is making the cabinet.  I am doing the electronics.  Since the last blog we’ve elected to limit the physical portion of the User Interface to an encoder with switch that controls on / off and volume.  With these simplifications it isn't necessary to write Python scripts and configuration can be done within MoOde.  Full control can still be done with a smart phone, tablet, or computer.

Block Diagram

Architecture

The MoOde architecture is shown in the diagram below.  Audio sources are in light blue across the top.  Local files, radio streams and UPnP have inputs to MPD in purple (more on that in a minute) as well as the ALSA (Advanced Linux Sound Architecture) DSP functions shown in light yellow.  Spotify and Airplay also have access to the DSP functions.  Bluetooth, LMS, and Roon Bridge are played directly from the configured audio device without DSP options.

MoOde Architecture

Credit:  BITLAB’S BYTES https://www.bitlab.nl/page_id=872

As can be seen in the architecture diagram, the primary control of local files and internet radio streams is done through MPD (Music Player Daemon) which is included in the MoOde download.  MPD is a server side application for playing music controlled by its network protocol.  Control of MPD is done with mpc and available commands are given here: https://helpmanual.io/help/mpc/.  They include methods for controlling volume, selecting files, etc. but not all commands seem to be available through MoOde.

A couple of methods were examined for incorporating volume control and on / off physical controls into our project before finally selecting an encoder.

USB HID Interface

USB HID (Human Interface Devices) codes are often built into keyboard devices.  There are a limited number accessible in MoOde.  One of my keyboards has mute, up volume, and down volume keys as shown in the image below.

Keyboard Volume Control

These keys can be mapped into MoOde and a keyboard or microcontroller with HID capability used for control.  The MoOde forum has instructions for incorporating “consumer control” HID codes using CircuitPython here: https://moodeaudio.org/forum/showthread.php?tid=4888&highlight=circuitpython.  A microcontroller or a momentary button switch can be used to turn the Raspberry Pi on and off using GPIO pins as described here: https://forums.raspberrypi.com/viewtopic.php?t=217442.

I tried it with my keyboard and it worked well but the functions available are limited.

MoOde SSH User Interface

The mpc commands can be issued through the MoOde user interface, web API, SSH command line, or from a script running on the Raspberry Pi.  Below is an example that increases the volume one increment using the web API:

              http://moode/command?cmd=vol.sh up 1

This is the same command using SSH located at m-> Configuration Settings -> Audio -> System -> Local Services -> SSH term server:

Set volume with SSH

The second call without specifying the volume direction and amount returns the current setting.  Using a Python script running on the Raspberry Pi and GPIO it would be possible to control volume and other functions.

This works well and gives access to mpc but since the most used functions are readily available from the MoOde user interface it isn’t something most users will access often.

MoOde Momentary Button Switch User Interface

The diagram below shows the pins that are already in use by the amplifier hat I'm using as well as the pin set aside for an on / off switch.

Amplifier Pin Usage

The mpc commands can be setup in the user interface to work with momentary button switches as found at m-> Configuration Settings -> Audio -> System -> Local Services -> GPIO button handler.  The pins use the BCM nomenclature and are pulled up.  Pins 27 and 22 were arbitrarily selected to control volume up and volume down respectively.

GPIO Pin Configuration

This worked as expected when tested by hooking up a dupont jumper to the desired pin and grounding it.  However, it seems out of place for a radio from the period we are using for inspiration as most used a rotary potentiometer.

Testing Buttons with Jumpers

Encoder

This is the option we elected to use.  Settings for rotary encoders to control volume are located at m-> Configuration Settings -> Audio -> Volume options -> Rotary encoder in MoOde:

Encoder Settings

I’ve left the default pin numbers at 23 and 24 for the moment and haven’t experimented with other settings.

The on / off switch in the encoder is wired to the Raspberry Pi and modifications made as described here.

Icing on the Cake

I made a first draft 3D print of the rocket and star that will be used for ornamentation on the front of the radio.  I expect we’ll have to fill, sand, and paint them with metallic paint to get the desired effect.

Rocket and Stars

Notes on Use

The instructions for adding a new radio station in the MoOde Forum are out of date.  The new method is to go to the Browse by “Radio Stations” landing page and click on the “+” button upper left.  Because of things like this I will put together a short user instruction sheet.

Next Steps

I plan to make a simple PCB for connecting the user controls to the Pi and then solder everything up before sending it to my brother. 

Useful Links

MoOde Landing Page:  https://moodeaudio.org/

Good Introduction to MoOde:  http://techzle.com/stream-music-with-raspberry-pi-and-moode-audio

MoOdeForum, adding radio stations: https://moodeaudio.org/forum/showthread.php?tid=116

Mpc commands: https://helpmanual.io/help/mpc/

MoOde Forum, connect hardware buttons: https://moodeaudio.org/forum/showthread.php?tid=198&highlight=%40Cyanoazimin

MoOde Forum, control Moode with Python: https://moodeaudio.org/forum/showthread.php?tid=1164&page=2&highlight=Web+api

MoOde Forum, control volume from command line: https://moodeaudio.org/forum/showthread.php?tid=1059&pid=7698#pid7698

MoOde Forum, change volume with pot / encoder: https://moodeaudio.org/forum/showthread.php?tid=4610&highlight=Volume+control

Raspberry Pi Forum, power on / off button for Pi: https://forums.raspberrypi.com/viewtopic.php?t=217442

MoOde Forum, USB Consumer Controller with CircuitPython: https://moodeaudio.org/forum/showthread.php?tid=4888&highlight=circuitpython

Moode Architecture: https://www.bitlab.nl/page_id=872

MPD User’s Manual: https://mpd.readthedocs.io/en/stable/user.html

  • Sign in to reply

Top Comments

  • genebren
    genebren over 4 years ago +1
    The radio project is making great progress! Keep up the good work.
  • beacon_dave
    beacon_dave over 4 years ago +1
    "...My brother now wants a small LED at the tail of the rocket to indicate power..." I was thinking that you could perhaps use an audio level indicator for this. Either a bullet meter that gets brighter…
  • beacon_dave
    beacon_dave over 4 years ago in reply to beacon_dave +1
    If the rocket /star was printed out of translucent material you could also make them glow or pulse.
Parents
  • beacon_dave
    beacon_dave over 4 years ago

    "...My brother now wants a small LED at the tail of the rocket to indicate power..."

    I was thinking that you could perhaps use an audio level indicator for this. Either a bullet meter that gets brighter with audio intensity or a flame effect that grows in length.  

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 4 years ago

    "...My brother now wants a small LED at the tail of the rocket to indicate power..."

    I was thinking that you could perhaps use an audio level indicator for this. Either a bullet meter that gets brighter with audio intensity or a flame effect that grows in length.  

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • beacon_dave
    beacon_dave over 4 years ago in reply to beacon_dave

    If the rocket /star was printed out of translucent material you could also make them glow or pulse. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 4 years ago in reply to beacon_dave

    Great ideas!  For sure I can make the make the material glow with the PLA I'm using for the prints.  That is a clever idea to use a bullet meter of have flame growth for a kind of VU meter. I have started looking into it.  I am aware of ways to use multiple LEDs as a digital VU but I'm looking for / trying to think of a circuit for a bullet meter with a 5V power rail.  I'm guessing I need a voltage controlled current source with high input impedance that will put out 0 to 10mA or so but averaged over some short period of time, say 20ms.  Need to rectify the audio also I suppose.