Member and Staff Blogs Simple Transistor Current Sources (and Sinks)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 4 May 2022 4:06 AM Date Created
  • Views 20776 views
  • Likes 16 likes
  • Comments 24 comments
  • transistor
  • current source
  • current sink
Related
Recommended

Simple Transistor Current Sources (and Sinks)

fmilburn
fmilburn
4 May 2022

Current sources and sinks have applications in many circuits and there are many ways to make them.  This blog is a brief introduction to single transistor current sources.   Horowitz and Hill cover this material in a more detailed fashion in The Art of Electronics 3rd Edition in section 2.2.6 Current Sources. 

The figure below shows four different single transistor circuits.  The NPN transistor circuits are current sinks while the PNP circuit is a current source.

Transistor Current Sources

Three current source biasing methods for the transistor are shown:

Figure A:  A voltage divider is used to set the Vb to 1.6 Volts.  This is acceptable as long as the voltage divider is stiff enough but can cause problems if the source voltage or load varies excessively.

Figure B: Forward-biased diodes are used to set Vb to 1.2V.

Figure C: A 5.6V zener diode is used to set Vb.

The biasing resistor is sized to allow the transistor to come into conduction.  Knowing the voltage at the base of the transistor, Vb, the emitter voltage is easily calculated since it will be 0.6V below Vb. Ohm's Law can then be used to size the emitter resistor for the desired current.  The base current will be ignored since it is much smaller than the collector current.

Using the circuit in Figure B as an example:

Bias Voltage:  The two silicon diodes have approximately a 0.6V drop each, for a total of 1.2V

Emitter Voltage: Base Voltage - 0.6V = 1.2 - 0.6 = 0.6V

Collector Current: Emitter Voltage / 56 Ohms = 0.6 / 56 = 10.7mA

Figure D: The circuit uses forward-biased diodes as in Figure B, but for a PNP current sink.

In the short 3-minute video below, the circuit in Figure B is demonstrated on a breadboard.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

These circuits perform well compared to a resistor biased from a fixed voltage such as commonly used for LEDs but as shown in the video they are not precision sources.  Improved circuits with additional transistors, op-amps, and IC current sources exist.  As an example, see the zero tempco constant current sources using the LM334Z in this design for a milliohm meter.  Horowitz and Hill also cover improved designs in The Art of Electronics.

  • Sign in to reply

Top Comments

  • Andrew J
    Andrew J over 4 years ago +1
    Good video Frank; can I call out the lack of err’s and umm’s and fluffed lines and the sound was fine. Loved the Lego men holding the wires, start he day with a smile. You could follow up with a video…
  • beacon_dave
    beacon_dave over 4 years ago in reply to fmilburn +1
    Yes, good gain structure helps. You ideally want your vocals to be lined up at around -18dBFS by the time you import into the editor. Unfortunately a lot of the consumer end kit doesn't provide useful…
  • dang74
    dang74 over 4 years ago +1
    One day I will sit down with the Art of Electronics while having SPICE open and ready. I figure running a few simulations of the example circuits will add to the experience and really nail concepts into…
Parents
  • DAB
    DAB over 4 years ago

    Transistors and their predecessor the triode, offered a lot of possible ways to configure the basic circuit for specific results.

    Needless to say, the final word on possible configurations has yet to be written.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 4 years ago

    Transistors and their predecessor the triode, offered a lot of possible ways to configure the basic circuit for specific results.

    Needless to say, the final word on possible configurations has yet to be written.