Member and Staff Blogs Stripper Shootout
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 1 Feb 2022 12:58 AM Date Created
  • Views 6377 views
  • Likes 13 likes
  • Comments 18 comments
  • doug wong
  • strippers
Related
Recommended

Stripper Shootout

dougw
dougw
1 Feb 2022

At most other places on the Internet "Stripper Shootout"  would have an entirely different meaning. Sunglasses

Here it is just a light blog providing members with an opportunity to post a picture of their favorite "strippers" and explain why they like them.

Below is a video of some "strippers" I have access to and a demonstration of the limits of my acting abilities .... As usual the cat steals the show....

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

For some reason I don't use the complex strippers I have. Maybe it is because they need to be adjusted and tested with every new wire size. That is a lot of overhead just to strip a wire. Maybe it is partly that they require a lot more physical effort to compress springs and overcome friction than is needed purely to strip insulation. This makes it difficult to feel exactly how much force is applied to squeezing the wire, cutting the insulation and pulling insulation free, and gaging the depth of cut, all of which can be important.

It is also curious to me that I don't remember where I got some of these strippers since I can remember exactly where I got virtually every other tool I own.

If you have a favorite set of strippers, feel free to post a picture or a comment below.

  • Sign in to reply

Top Comments

  • wolfgangfriedrich
    wolfgangfriedrich over 4 years ago +1
    My favourite set is one, that I just got as a Secret Santa present. And not only because it is my only one, but there is really no adjustment needed from wire size 12 to 28. Just feed and strip. community…
  • scottiebabe
    scottiebabe over 4 years ago +1
    +10 for the intro. LOL As a child I used scissors for years with those 100-in-1 spring terminal kits. Which work fine for taking the insulation off solid core wire. It is the nasty nick they leave that…
  • robogary
    robogary over 4 years ago +1
    made me look :-)
Parents
  • aspork42
    aspork42 over 4 years ago

    If you've never used cable strippers, you don't know how much you're missing!

    We use these at work to pull the jackets off of multi-conductor cable. They are super easy to use - slip the cable into the notch, then rotate the tool around the cable. The little tiny blade cuts the jacket neatly. You can then turn the handle 90 degrees and slit the jacket lengthwise as you pull the cable out. I know that this description might be confusing... sorry! It takes only seconds to strip a multi-conductor cable. This Greenlee is pricy, but there are less expensive options out there. If you strip a lot of cable, this is something to consider.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • aspork42
    aspork42 over 4 years ago

    If you've never used cable strippers, you don't know how much you're missing!

    We use these at work to pull the jackets off of multi-conductor cable. They are super easy to use - slip the cable into the notch, then rotate the tool around the cable. The little tiny blade cuts the jacket neatly. You can then turn the handle 90 degrees and slit the jacket lengthwise as you pull the cable out. I know that this description might be confusing... sorry! It takes only seconds to strip a multi-conductor cable. This Greenlee is pricy, but there are less expensive options out there. If you strip a lot of cable, this is something to consider.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 4 years ago in reply to aspork42

    Cool, I've used coax strippers, but never seen multiconductor strippers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to aspork42

    Nice! There is a compact version that is less flexible (it cannot slit lengthways), I use it for coax, Main disadvantage of the one below however is that it is screw-set, and it takes so long fine-tuning the blade setting (tens of minutes!) that it's really only for set-and-forget for one cable thickness : ( so the one below rarely gets used. There's also a Knipex ErgoStrip which is like a lower-cost version of the Greenlee one, but the Greenlee one looks to be of noticeably better quality.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to aspork42

    this description might be confusing... sorry!

    Yes it was confusing - but correct :). There's a video that shows what you write: