Member and Staff Blogs Stripper Shootout
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 1 Feb 2022 12:58 AM Date Created
  • Views 6384 views
  • Likes 13 likes
  • Comments 18 comments
  • doug wong
  • strippers
Related
Recommended

Stripper Shootout

dougw
dougw
1 Feb 2022

At most other places on the Internet "Stripper Shootout"  would have an entirely different meaning. Sunglasses

Here it is just a light blog providing members with an opportunity to post a picture of their favorite "strippers" and explain why they like them.

Below is a video of some "strippers" I have access to and a demonstration of the limits of my acting abilities .... As usual the cat steals the show....

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

For some reason I don't use the complex strippers I have. Maybe it is because they need to be adjusted and tested with every new wire size. That is a lot of overhead just to strip a wire. Maybe it is partly that they require a lot more physical effort to compress springs and overcome friction than is needed purely to strip insulation. This makes it difficult to feel exactly how much force is applied to squeezing the wire, cutting the insulation and pulling insulation free, and gaging the depth of cut, all of which can be important.

It is also curious to me that I don't remember where I got some of these strippers since I can remember exactly where I got virtually every other tool I own.

If you have a favorite set of strippers, feel free to post a picture or a comment below.

  • Sign in to reply

Top Comments

  • wolfgangfriedrich
    wolfgangfriedrich over 4 years ago +1
    My favourite set is one, that I just got as a Secret Santa present. And not only because it is my only one, but there is really no adjustment needed from wire size 12 to 28. Just feed and strip. community…
  • scottiebabe
    scottiebabe over 4 years ago +1
    +10 for the intro. LOL As a child I used scissors for years with those 100-in-1 spring terminal kits. Which work fine for taking the insulation off solid core wire. It is the nasty nick they leave that…
  • robogary
    robogary over 4 years ago +1
    made me look :-)
Parents
  • Gough Lui
    Gough Lui over 4 years ago

    I used to use a pair of cheap plastic automatic wire strippers but I found their cutting jaws to be slightly uneven and not much chop on larger cables.

    But over a decade ago, I discovered the Xcelite 101SNV, a decidedly manual sort of wire stripper, but one which works on stuff like mains cable down to even the finer stranded 28AWG wire. The spring loaded auto open is nice, and if you have some 'feeling' in your hands, you learn to strip wire consistently without marring the conductors. It's also near impossible to break and works as a cutter too on the flat surfaces either side of the 'wedge' cutout. Simple but effective, and almost impossible to destroy.

    https://au.element14.com/xcelite/101sv/wire-strippercutter-self-open/dp/440747

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Gough Lui
    Gough Lui over 4 years ago

    I used to use a pair of cheap plastic automatic wire strippers but I found their cutting jaws to be slightly uneven and not much chop on larger cables.

    But over a decade ago, I discovered the Xcelite 101SNV, a decidedly manual sort of wire stripper, but one which works on stuff like mains cable down to even the finer stranded 28AWG wire. The spring loaded auto open is nice, and if you have some 'feeling' in your hands, you learn to strip wire consistently without marring the conductors. It's also near impossible to break and works as a cutter too on the flat surfaces either side of the 'wedge' cutout. Simple but effective, and almost impossible to destroy.

    https://au.element14.com/xcelite/101sv/wire-strippercutter-self-open/dp/440747

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 4 years ago in reply to Gough Lui

    Nice to see someone else using the same type I prefer. I have a set that is still working well after more than 40 years. I like to have total "feel" control of how deeply they cut into the insulation, because different insulation materials need different depths of cut, and some insulations cuts benefit from twisting the stripper blades in one or more axes.