Member and Staff Blogs Thanks Santa!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: scottiebabe
  • Date Created: 30 Jan 2022 4:35 PM Date Created
  • Views 2148 views
  • Likes 15 likes
  • Comments 5 comments
Related
Recommended

Thanks Santa!

scottiebabe
scottiebabe
30 Jan 2022

A mystery Newark package appeared on my doorstep this past week. I wonder what it could be? 

 

It’s a gift from the wonderful dychen and my secret Santa!

 

Remote controlled wireless touch lights!

 image

A gift where batteries are included. Look at how many alkaline cells are included in this package:

 image

With 18 AA and 2 AAA alkaline cells, this kit weighs several pounds. I love the fact that the batteries are included.

The lights didn’t come preprogramed for the RF remote, but pairing them is simple. You enter pairing the pairing mode by inserting the final battery with the front cover switch depressed. Then just press on of the remotes buttons and the light is paired to the remote. Here are the lights all powered up:

 image

Teardown

Here is a look at one of the lights up close:

 image

Each light has a twist lock back panel that is indented to be mounted to a surface with double sided adhesive pads. Each light requires 3 AA cells:

 image

Taking the front cover off you can see how the front lens is sprung with 4 plastic tabs:

 image

Not much to see on top side of the printed circuit board…

 image

The bottom side is much more interesting:

image

Only 2 zero-ohm jumper links were needed for this single-sided PCB.  The solder mask is noticeably misaligned to the copper pads in many locations. Overall, a pretty nice little 2.4 GHz remote controlled touch light.

 Here is a rough schematic of the touch light.

 image

Mostly mystery parts, but the Holtek LDO specifies a typical quiescent current of 2 uA, which is nice to see in a battery powered product.

Secret code

I probed the I2C bus while pairing the RF remote. The MCU stores a value of 0xE0 into the 2kbit serial EEPROM at address 0x00.

image

Subsequently, when the light is powered up normally, it reads this magic code from the serial  EEPROM:

 image

Plus an additionally byte, not sure why. 

Power Consumption

With the light turned off, the quiescent current is approximately 300 uA. So, even if you don’t ever use these lights, you would deplete 2000 mAh rated AA cells in less than a year. With light running the LEDs at full intensity and a 4.5V battery voltage the operating current is 138 mA. The dim mode current is 76 mA.

The MCU wakes up and listens for remote commands at approximately 5 Hz:

image

The MCU and RF module are only listening for RF packets for approximately 2 ms before going back to sleep:

image

I didn’t end up getting a real-time spectrum analyzer (or SDR) for Christmas, so the 2.4 GHz signaling will have to be left as a mystery.

Never the less, this is an extremely thoughtful gift and really nice wireless touch light. And, will make a great addition to my closet Blush.

Best wishes to all who make e14 wonderful.

Update: RF Remote

Here is a photo of the internals of the RF remote which operates on 2 series AAA cells:

image image

The interesting observations here are:

  • There is a 12 MHz crystal in a 2mm x 6mm cylinder can (similar to 32 kHz tuning fork crystals)  
  • They used silkscreen as solder mask to route traces between the pads of the SOIC-14 MCU

  • Sign in to reply
  • beacon_dave
    beacon_dave over 4 years ago in reply to scottiebabe

    Replace the LEDs with 2kW halogen lamps. 

    May need a few more batteries but it should warm you up. Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to dubbie

    Four buttons. Hmmm... forward, back, left, right. what more do you need ? Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 4 years ago in reply to dubbie
    This comment was deleted.
    • Cancel
    • More
    • Cancel
  • dubbie
    dubbie over 4 years ago

    A nice secret gift. I wonder what else they can be converted to control?

    Dubbie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 4 years ago

    Nice surprise, and a really insightful teardown.