Member and Staff Blogs What's new in fairy tech?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: scottiebabe
  • Date Created: 16 Nov 2023 1:35 AM Date Created
  • Views 2650 views
  • Likes 11 likes
  • Comments 19 comments
Related
Recommended

What's new in fairy tech?

scottiebabe
scottiebabe
16 Nov 2023

The first set of fairy lights I purchased a few years ago had a very rudimentary embodiment. Just two AA batteries, an on/off switch, and a string of miniature LEDs on enamel wire.

image

I love the simplicity of the design... The design works well enough with disposable alkaline batteries. However recharge cells don't work very well on their own, as their combided state of charge voltage very quickly drops below the forward voltage of the white LEDs.

Fairy Tech 2.0

Browsing at the dollar store today, I found some new fairy lights which included some circuitry on a PCB. What could it be?

image image

Same general look and feel as before.

image

Now included is a three position switch!

image

The mysterious PCB

image

No sign of an inductor anywhere Disappointed. Just a

- 8-pin MCU?

- Watch crystal

- SPDT Slide switch

image

Fairy Tech 3.0

I can upgrade this new set of fairy lights with a boost converter module capable of operating of a single alkaline/Ni-MH cell

image

Module based on ME2188 https://file.elecfans.com/web2/M00/64/78/poYBAGMHOg-APsG0AAge4TQOpd0961.pdf 

I bought a value pack awhile back thinking I would receive a selection of different output voltages. Nope, I got a bag of identical modules and each has a nominal output voltage of 5V. So, I added an additional 50 Ohm series resistor to limit the current to approximately 40 mA.

image

I am taking a bit of a gamble assuming the MCU is 5V rated. If it gives up the ghost, I'll replace it too.

image

All for now.

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 2 years ago in reply to scottiebabe +1
    Out of the box they can also sometimes be a bit too bright for fast lenses with wide open apertures. Arducam do a low-cost F1.6 C-Mount lens which can be used with the likes of a R-Pi HQ camera for bokeh…
Parents
  • dougw
    dougw over 2 years ago

    So what does the original PCB do? Modulate the power to prevent LED over-current and extend battery life?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to dougw

    The LEDs are being low side switched by an output pin. There isn't any PWM modulation. The limited drive strength of the MCU output is adding some additional series resistance between the batteries and the LEDs. This would result in a slightly longer runtime when lit. 

    The only new function I can see, is the 6hr timer. Where the MCU switches the LEDs on for 6 hours then off for 18 hours, before the cycle repeats. Just like in many LED candles. Though most of those use three batteries in series, which has a greater output voltage than the forward voltage of white LEDs even when the batteries are depleted.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • scottiebabe
    scottiebabe over 2 years ago in reply to dougw

    The LEDs are being low side switched by an output pin. There isn't any PWM modulation. The limited drive strength of the MCU output is adding some additional series resistance between the batteries and the LEDs. This would result in a slightly longer runtime when lit. 

    The only new function I can see, is the 6hr timer. Where the MCU switches the LEDs on for 6 hours then off for 18 hours, before the cycle repeats. Just like in many LED candles. Though most of those use three batteries in series, which has a greater output voltage than the forward voltage of white LEDs even when the batteries are depleted.